Part Number: AM2434
Other Parts Discussed in Thread: AM2431, AM2634,
Hi,
I want to be able to sync the clocks of two devices using IEEE TSN or IEEE 1588 standard with a jitter of less than 100 nanoseconds. I see that the AM243x series of MCUs supports TSN but I am concerned about the speed of these microcontrollers at 1 Gbps speeds.
Will the AM2434 be fast enough to achieve a jitter of less than 100 ns at 1 Gbps Ethernet speeds? What about the AM2431 or 2432?
I also see that many of TI's Sitara MPUs support TSN and are much faster than their MCU counterparts. I was looking at the AM652x and AM641x MPUs. I was interested in using the MCU over the MPUs because of the reduced complexity (utilizing TI-Clang & CCS vs. Linux) and the reduced FCCSP (ALX) package size (293 pin) of the AM243x MCUs.
For my application requirements: Gigabit Ethernet (1000 Mbps) speeds and TSN synchronization with a jitter of less than 100 ns, what would you suggest I use? The MCU or MPU listed above? Or does anyone have a different suggestion? Please note smaller and lower cost are better. My only other requirement for the processor/controller would be a couple of SPI & UART ports. I do not need PCIe, etc. I will be utilizing an external 1000BaseT1 PHY to convert to the required MDI.