Part Number: TMS570LS1227
Other Parts Discussed in Thread: HALCOGEN
Tool/software:
/**
* @file tms570_eth_driver.c
* @brief TMS570 Ethernet MAC driver
*
* @section License
*
* SPDX-License-Identifier: GPL-2.0-or-later
*
* Copyright (C) 2010-2024 Oryx Embedded SARL. All rights reserved.
*
* This file is part of CycloneTCP Open.
*
* This program is free software; you can redistribute it and/or
* modify it under the terms of the GNU General Public License
* as published by the Free Software Foundation; either version 2
* of the License, or (at your option) any later version.
*
* This program is distributed in the hope that it will be useful,
* but WITHOUT ANY WARRANTY; without even the implied warranty of
* MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
* GNU General Public License for more details.
*
* You should have received a copy of the GNU General Public License
* along with this program; if not, write to the Free Software Foundation,
* Inc., 51 Franklin Street, Fifth Floor, Boston, MA 02110-1301, USA.
*
* @author Oryx Embedded SARL (www.oryx-embedded.com)
* @version 2.4.2
**/
//Switch to the appropriate trace level
#define TRACE_LEVEL NIC_TRACE_LEVEL
//Platform-specific dependencies
#if defined(_TMS570LC43x_)
#include "hl_hw_reg_access.h"
#include "hl_hw_emac.h"
#include "hl_hw_emac_ctrl.h"
#include "hl_hw_mdio.h"
#include "hl_gio.h"
#include "hl_sys_vim.h"
#else
#include "hw_reg_access.h"
#include "hw_emac.h"
#include "hw_emac_ctrl.h"
#include "hw_mdio.h"
#include "gio.h"
#include "sys_vim.h"
#endif
//Dependencies
#include "core/net.h"
#include "drivers/mac/tms570_eth_driver.h"
#include "debug.h"
//MDIO input clock frequency
#define MDIO_INPUT_CLK 75000000
//MDIO output clock frequency
#define MDIO_OUTPUT_CLK 1000000
//Byte-swapped read/write accesses to CPPI memory?
#if defined(_TMS570LC43x_)
#define CPPI_SWAP(x) swapInt32((uint32_t) (x))
#else
#define CPPI_SWAP(x) ((uint32_t) (x))
#endif
//Underlying network interface
static NetInterface *nicDriverInterface;
//IAR EWARM compiler?
#if defined(__ICCARM__)
//Transmit buffer
#pragma data_alignment = 4
#pragma location = TMS570_ETH_RAM_SECTION
static uint8_t txBuffer[TMS570_ETH_TX_BUFFER_COUNT][TMS570_ETH_TX_BUFFER_SIZE];
//Receive buffer
#pragma data_alignment = 4
#pragma location = TMS570_ETH_RAM_SECTION
static uint8_t rxBuffer[TMS570_ETH_RX_BUFFER_COUNT][TMS570_ETH_RX_BUFFER_SIZE];
//Transmit buffer descriptors
#pragma data_alignment = 4
#pragma location = TMS570_ETH_RAM_CPPI_SECTION
static Tms570TxBufferDesc txBufferDesc[TMS570_ETH_TX_BUFFER_COUNT];
//Receive buffer descriptors
#pragma data_alignment = 4
#pragma location = TMS570_ETH_RAM_CPPI_SECTION
static Tms570RxBufferDesc rxBufferDesc[TMS570_ETH_RX_BUFFER_COUNT];
//GCC compiler?
#else
//Transmit buffer
static uint8_t txBuffer[TMS570_ETH_TX_BUFFER_COUNT][TMS570_ETH_TX_BUFFER_SIZE]
__attribute__((aligned(4), __section__(TMS570_ETH_RAM_SECTION)));
//Receive buffer
static uint8_t rxBuffer[TMS570_ETH_RX_BUFFER_COUNT][TMS570_ETH_RX_BUFFER_SIZE]
__attribute__((aligned(4), __section__(TMS570_ETH_RAM_SECTION)));
//Transmit buffer descriptors
static Tms570TxBufferDesc txBufferDesc[TMS570_ETH_TX_BUFFER_COUNT]
__attribute__((aligned(4), __section__(TMS570_ETH_RAM_CPPI_SECTION)));
//Receive buffer descriptors
static Tms570RxBufferDesc rxBufferDesc[TMS570_ETH_RX_BUFFER_COUNT]
__attribute__((aligned(4), __section__(TMS570_ETH_RAM_CPPI_SECTION)));
#endif
//Pointer to the current TX buffer descriptor
static Tms570TxBufferDesc *txCurBufferDesc;
//Pointer to the current RX buffer descriptor
static Tms570RxBufferDesc *rxCurBufferDesc;
/**
* @brief TMS570 Ethernet MAC driver
**/
const NicDriver tms570EthDriver =
{
NIC_TYPE_ETHERNET,
ETH_MTU,
tms570EthInit,
tms570EthTick,
tms570EthEnableIrq,
tms570EthDisableIrq,
tms570EthEventHandler,
tms570EthSendPacket,
tms570EthUpdateMacAddrFilter,
tms570EthUpdateMacConfig,
tms570EthWritePhyReg,
tms570EthReadPhyReg,
FALSE,
TRUE,
TRUE,
FALSE
};
/**
* @brief TMS570 Ethernet MAC initialization
* @param[in] interface Underlying network interface
* @return Error code
**/
error_t tms570EthInit(NetInterface *interface)
{
error_t error;
uint_t channel;
uint32_t temp;
//Debug message
TRACE_INFO("Initializing TMS570 Ethernet MAC...\r\n");
//Save underlying network interface
nicDriverInterface = interface;
//Select the interface mode (MII/RMII) and configure pin muxing
tms570EthInitGpio(interface);
//Reset the EMAC control module
EMAC_CTRL_SOFTRESET_R = EMAC_SOFTRESET_SOFTRESET;
//Wait for the reset to complete
while((EMAC_CTRL_SOFTRESET_R & EMAC_SOFTRESET_SOFTRESET) != 0)
{
}
//Reset the EMAC module
EMAC_SOFTRESET_R = EMAC_SOFTRESET_SOFTRESET;
//Wait for the reset to complete
while((EMAC_SOFTRESET_R & EMAC_SOFTRESET_SOFTRESET) != 0)
{
}
//Calculate the MDC clock divider to be used
temp = (MDIO_INPUT_CLK / MDIO_OUTPUT_CLK) - 1;
//Initialize MDIO interface
MDIO_CONTROL_R = MDIO_CONTROL_ENABLE |
MDIO_CONTROL_FAULTENB | (temp & MDIO_CONTROL_CLKDIV);
//Valid Ethernet PHY or switch driver?
if(interface->phyDriver != NULL)
{
//Ethernet PHY initialization
error = interface->phyDriver->init(interface);
}
else if(interface->switchDriver != NULL)
{
//Ethernet switch initialization
error = interface->switchDriver->init(interface);
}
else
{
//The interface is not properly configured
error = ERROR_FAILURE;
}
//Any error to report?
if(error)
{
return error;
}
//Clear the control registers
EMAC_MACCONTROL_R = 0;
EMAC_RXCONTROL_R = 0;
EMAC_TXCONTROL_R = 0;
//Initialize all 16 header descriptor pointer registers to 0
for(channel = EMAC_CH0; channel <= EMAC_CH7; channel++)
{
//TX head descriptor pointer
EMAC_TXHDP_R(channel) = 0;
//TX completion pointer
EMAC_TXCP_R(channel) = 0;
//RX head descriptor pointer
EMAC_RXHDP_R(channel) = 0;
//RX completion pointer
EMAC_RXCP_R(channel) = 0;
}
//Set the upper 32 bits of the source MAC address
EMAC_MACSRCADDRHI_R = interface->macAddr.b[0] |
(interface->macAddr.b[1] << 8) |
(interface->macAddr.b[2] << 16) |
(interface->macAddr.b[3] << 24);
//Set the lower 16 bits of the source MAC address
EMAC_MACSRCADDRLO_R = interface->macAddr.b[4] |
(interface->macAddr.b[5] << 8);
//Write the channel number to the MAC index register
EMAC_MACINDEX_R = EMAC_CH0;
//Set the upper 32 bits of the destination MAC address
EMAC_MACADDRHI_R = interface->macAddr.b[0] |
(interface->macAddr.b[1] << 8) |
(interface->macAddr.b[2] << 16) |
(interface->macAddr.b[3] << 24);
//Set the lower 16 bits of the destination MAC address
temp = interface->macAddr.b[4] |
(interface->macAddr.b[5] << 8);
//Use the current MAC address to match incoming packet addresses
EMAC_MACADDRLO_R = EMAC_MACADDRLO_VALID | EMAC_MACADDRLO_MATCHFILT |
(EMAC_CH0 << EMAC_MACADDRLO_CHANNEL_SHIFT) | temp;
//Be sure to program all eight MAC address registers, whether the
//receive channel is to be enabled or not
for(channel = EMAC_CH1; channel <= EMAC_CH7; channel++)
{
//Write the channel number to the MAC index register
EMAC_MACINDEX_R = channel;
//The MAC address is not valid
EMAC_MACADDRLO_R = (channel << EMAC_MACADDRLO_CHANNEL_SHIFT);
}
//Clear the MAC address hash registers
EMAC_MACHASH1_R = 0;
EMAC_MACHASH2_R = 0;
//The RX buffer offset must be initialized to zero
EMAC_RXBUFFEROFFSET_R = 0;
//Clear all unicast channels
EMAC_RXUNICASTCLEAR_R = 0xFF;
//Accept unicast frames
EMAC_RXUNICASTSET_R |= (1 << EMAC_CH0);
//Received CRC is transferred to memory for all channels
EMAC_RXMBPENABLE_R = EMAC_RXMBPENABLE_RXPASSCRC;
//Accept broadcast frames
EMAC_RXMBPENABLE_R |= EMAC_RXMBPENABLE_RXBROADEN |
(EMAC_CH0 << EMAC_RXMBPENABLE_RXBROADCH_SHIFT);
//Accept hash matching multicast frames
EMAC_RXMBPENABLE_R |= EMAC_RXMBPENABLE_RXMULTEN |
(EMAC_CH0 << EMAC_RXMBPENABLE_RXMULTCH_SHIFT);
//Register TX interrupt handler
vimChannelMap(TMS570_ETH_TX_IRQ_CHANNEL, TMS570_ETH_TX_IRQ_CHANNEL,
(t_isrFuncPTR) tms570EthTxIrqHandler);
//Register RX interrupt handler
vimChannelMap(TMS570_ETH_RX_IRQ_CHANNEL, TMS570_ETH_RX_IRQ_CHANNEL,
(t_isrFuncPTR) tms570EthRxIrqHandler);
//Clear all unused channel interrupt bits
EMAC_TXINTMASKCLEAR_R = 0xFF;
EMAC_RXINTMASKCLEAR_R = 0xFF;
//Enable the receive and transmit channel interrupt bits
EMAC_TXINTMASKSET_R = (1 << EMAC_CH0);
EMAC_RXINTMASKSET_R = (1 << EMAC_CH0);
//Configure TX and RX buffer descriptors
tms570EthInitBufferDesc(interface);
//Write the RX DMA head descriptor pointer
EMAC_RXHDP_R(EMAC_CH0) = (uint32_t) rxCurBufferDesc;
//Enable the receive and transmit DMA controllers
EMAC_TXCONTROL_R = EMAC_TXCONTROL_TXEN;
EMAC_RXCONTROL_R = EMAC_RXCONTROL_RXEN;
//Enable TX and RX
EMAC_MACCONTROL_R = EMAC_MACCONTROL_GMIIEN;
//Enable TX and RX completion interrupts
EMAC_CTRL_CnTXEN_R(EMAC_CORE0) |= (1 << EMAC_CH0);
EMAC_CTRL_CnRXEN_R(EMAC_CORE0) |= (1 << EMAC_CH0);
//Accept any packets from the upper layer
osSetEvent(&interface->nicTxEvent);
//Successful initialization
return NO_ERROR;
}
/**
* @brief GPIO configuration
* @param[in] interface Underlying network interface
**/
__weak_func void tms570EthInitGpio(NetInterface *interface)
{
//LAUNCHXL2-570LC43 evaluation board?
#if defined(USE_LAUNCHXL2_570LC43)
//Configure PHY_INT (PA_3) as an input
gioPORTA->DIR &= ~(1 << 3);
gioPORTA->PSL |= (1 << 3);
gioPORTA->PULDIS &= ~(1 << 3);
//Configure PHY_RST (PA_4) as an output
gioPORTA->DIR |= (1 << 4);
gioPORTA->PDR &= ~(1 << 4);
//Reset PHY transceiver
gioPORTA->DCLR = (1 << 4);
sleep(10);
gioPORTA->DSET = (1 << 4);
sleep(10);
#endif
}
/**
* @brief Initialize buffer descriptor lists
* @param[in] interface Underlying network interface
**/
void tms570EthInitBufferDesc(NetInterface *interface)
{
uint_t i;
uint_t nextIndex;
uint_t prevIndex;
//Initialize TX buffer descriptor list
for(i = 0; i < TMS570_ETH_TX_BUFFER_COUNT; i++)
{
//Index of the next buffer
nextIndex = (i + 1) % TMS570_ETH_TX_BUFFER_COUNT;
//Index of the previous buffer
prevIndex = (i + TMS570_ETH_TX_BUFFER_COUNT - 1) % TMS570_ETH_TX_BUFFER_COUNT;
//Next descriptor pointer
txBufferDesc[i].word0 = CPPI_SWAP(NULL);
//Buffer pointer
txBufferDesc[i].word1 = CPPI_SWAP(txBuffer[i]);
//Buffer offset and buffer length
txBufferDesc[i].word2 = CPPI_SWAP(0);
//Status flags and packet length
txBufferDesc[i].word3 = CPPI_SWAP(0);
//Form a doubly linked list
txBufferDesc[i].next = &txBufferDesc[nextIndex];
txBufferDesc[i].prev = &txBufferDesc[prevIndex];
}
//Point to the very first descriptor
txCurBufferDesc = &txBufferDesc[0];
//Mark the end of the queue
txCurBufferDesc->prev->word3 = CPPI_SWAP(EMAC_TX_WORD3_SOP |
EMAC_TX_WORD3_EOP | EMAC_TX_WORD3_EOQ);
//Initialize RX buffer descriptor list
for(i = 0; i < TMS570_ETH_RX_BUFFER_COUNT; i++)
{
//Index of the next buffer
nextIndex = (i + 1) % TMS570_ETH_RX_BUFFER_COUNT;
//Index of the previous buffer
prevIndex = (i + TMS570_ETH_RX_BUFFER_COUNT - 1) % TMS570_ETH_RX_BUFFER_COUNT;
//Next descriptor pointer
rxBufferDesc[i].word0 = CPPI_SWAP(&rxBufferDesc[nextIndex]);
//Buffer pointer
rxBufferDesc[i].word1 = CPPI_SWAP(rxBuffer[i]);
//Buffer offset and buffer length
rxBufferDesc[i].word2 = CPPI_SWAP(TMS570_ETH_RX_BUFFER_SIZE);
//Status flags and packet length
rxBufferDesc[i].word3 = CPPI_SWAP(EMAC_RX_WORD3_OWNER);
//Form a doubly linked list
rxBufferDesc[i].next = &rxBufferDesc[nextIndex];
rxBufferDesc[i].prev = &rxBufferDesc[prevIndex];
}
//Point to the very first descriptor
rxCurBufferDesc = &rxBufferDesc[0];
//Mark the end of the queue
// rxCurBufferDesc->prev->word0 = CPPI_SWAP(NULL);
}
/**
* @brief TMS570 Ethernet MAC timer handler
*
* This routine is periodically called by the TCP/IP stack to handle periodic
* operations such as polling the link state
*
* @param[in] interface Underlying network interface
**/
void tms570EthTick(NetInterface *interface)
{
//Valid Ethernet PHY or switch driver?
if(interface->phyDriver != NULL)
{
//Handle periodic operations
interface->phyDriver->tick(interface);
}
else if(interface->switchDriver != NULL)
{
//Handle periodic operations
interface->switchDriver->tick(interface);
}
else
{
//Just for sanity
}
//Misqueued buffer condition?
if(CPPI_SWAP(rxCurBufferDesc->word3) & EMAC_RX_WORD3_OWNER)
{
if(EMAC_RXHDP_R(EMAC_CH0) == 0)
{
//The host acts on the misqueued buffer condition by writing the added
//buffer descriptor address to the appropriate RX DMA head descriptor
//pointer
EMAC_RXHDP_R(EMAC_CH0) = (uint32_t) rxCurBufferDesc;
}
}
}
/**
* @brief Enable interrupts
* @param[in] interface Underlying network interface
**/
void tms570EthEnableIrq(NetInterface *interface)
{
//Enable Ethernet MAC interrupts
vimEnableInterrupt(TMS570_ETH_TX_IRQ_CHANNEL, SYS_IRQ);
vimEnableInterrupt(TMS570_ETH_RX_IRQ_CHANNEL, SYS_IRQ);
//Valid Ethernet PHY or switch driver?
if(interface->phyDriver != NULL)
{
//Enable Ethernet PHY interrupts
interface->phyDriver->enableIrq(interface);
}
else if(interface->switchDriver != NULL)
{
//Enable Ethernet switch interrupts
interface->switchDriver->enableIrq(interface);
}
else
{
//Just for sanity
}
}
/**
* @brief Disable interrupts
* @param[in] interface Underlying network interface
**/
void tms570EthDisableIrq(NetInterface *interface)
{
//Disable Ethernet MAC interrupts
vimDisableInterrupt(TMS570_ETH_TX_IRQ_CHANNEL);
vimDisableInterrupt(TMS570_ETH_RX_IRQ_CHANNEL);
//Valid Ethernet PHY or switch driver?
if(interface->phyDriver != NULL)
{
//Disable Ethernet PHY interrupts
interface->phyDriver->disableIrq(interface);
}
else if(interface->switchDriver != NULL)
{
//Disable Ethernet switch interrupts
interface->switchDriver->disableIrq(interface);
}
else
{
//Just for sanity
}
}
/**
* @brief Ethernet MAC transmit interrupt
**/
#if defined(__ICCARM__)
__irq __arm
#else
#pragma CODE_STATE(tms570EthTxIrqHandler, 32)
#pragma INTERRUPT(tms570EthTxIrqHandler, IRQ)
#endif
void tms570EthTxIrqHandler(void)
{
bool_t flag;
uint32_t status;
uint32_t temp;
Tms570TxBufferDesc *p;
//Interrupt service routine prologue
osEnterIsr();
//This flag will be set if a higher priority task must be woken
flag = FALSE;
//Read the C0TXSTAT register to determine which channels caused the interrupt
status = EMAC_CTRL_C0TXSTAT_R;
//Packet transmitted on channel 0?
if(status & (1 << EMAC_CH0))
{
//Point to the buffer descriptor
p = (Tms570TxBufferDesc *) EMAC_TXCP_R(EMAC_CH0);
//Read the status flags
temp = CPPI_SWAP(p->word3) & (EMAC_TX_WORD3_SOP | EMAC_TX_WORD3_EOP |
EMAC_TX_WORD3_OWNER | EMAC_TX_WORD3_EOQ);
//Misqueued buffer condition?
if(temp == (EMAC_TX_WORD3_SOP | EMAC_TX_WORD3_EOP | EMAC_TX_WORD3_EOQ))
{
//Check whether the next descriptor pointer is non-zero
if(CPPI_SWAP(p->word0) != 0)
{
//The host corrects the misqueued buffer condition by writing the
//misqueued packet�s buffer descriptor address to the appropriate
//TX DMA head descriptor pointer
EMAC_TXHDP_R(EMAC_CH0) = CPPI_SWAP(p->word0);
}
}
//Write the TX completion pointer
EMAC_TXCP_R(EMAC_CH0) = (uint32_t) p;
//Check whether the TX buffer is available for writing
if((CPPI_SWAP(txCurBufferDesc->word3) & EMAC_TX_WORD3_OWNER) == 0)
{
//Notify the TCP/IP stack that the transmitter is ready to send
flag |= osSetEventFromIsr(&nicDriverInterface->nicTxEvent);
}
}
//Write the DMA end of interrupt vector
EMAC_MACEOIVECTOR_R = EMAC_MACEOIVECTOR_C0TX;
//Interrupt service routine epilogue
osExitIsr(flag);
}
/**
* @brief Ethernet MAC receive interrupt
**/
#if defined(__ICCARM__)
__irq __arm
#else
#pragma CODE_STATE(tms570EthRxIrqHandler, 32)
#pragma INTERRUPT(tms570EthRxIrqHandler, IRQ)
#endif
void tms570EthRxIrqHandler(void)
{
bool_t flag;
uint32_t status;
//Interrupt service routine prologue
osEnterIsr();
//This flag will be set if a higher priority task must be woken
flag = FALSE;
//Read the C0RXSTAT register to determine which channels caused the interrupt
status = EMAC_CTRL_C0RXSTAT_R;
//Packet received on channel 0?
if(status & (1 << EMAC_CH0))
{
//Disable RX interrupts
EMAC_CTRL_CnRXEN_R(EMAC_CORE0) &= ~(1 << EMAC_CH0);
//Set event flag
nicDriverInterface->nicEvent = TRUE;
//Notify the TCP/IP stack of the event
flag |= osSetEventFromIsr(&netEvent);
}
//Write the DMA end of interrupt vector
EMAC_MACEOIVECTOR_R = EMAC_MACEOIVECTOR_C0RX;
//Interrupt service routine epilogue
osExitIsr(flag);
}
/**
* @brief TMS570 Ethernet MAC event handler
* @param[in] interface Underlying network interface
**/
void tms570EthEventHandler(NetInterface *interface)
{
error_t error;
//Process all pending packets
do
{
//Read incoming packet
error = tms570EthReceivePacket(interface);
//No more data in the receive buffer?
} while(error != ERROR_BUFFER_EMPTY);
//Re-enable RX interrupts
EMAC_CTRL_CnRXEN_R(EMAC_CORE0) |= (1 << EMAC_CH0);
}
/**
* @brief Send a packet
* @param[in] interface Underlying network interface
* @param[in] buffer Multi-part buffer containing the data to send
* @param[in] offset Offset to the first data byte
* @param[in] ancillary Additional options passed to the stack along with
* the packet
* @return Error code
**/
error_t tms570EthSendPacket(NetInterface *interface,
const NetBuffer *buffer, size_t offset, NetTxAncillary *ancillary)
{
size_t length;
uint32_t temp;
//Retrieve the length of the packet
length = netBufferGetLength(buffer) - offset;
//Check the frame length
if(length > TMS570_ETH_TX_BUFFER_SIZE)
{
//The transmitter can accept another packet
osSetEvent(&interface->nicTxEvent);
//Report an error
return ERROR_INVALID_LENGTH;
}
//Make sure the current buffer is available for writing
if(CPPI_SWAP(txCurBufferDesc->word3) & EMAC_TX_WORD3_OWNER)
{
return ERROR_FAILURE;
}
//Mark the end of the queue with a NULL pointer
txCurBufferDesc->word0 = CPPI_SWAP(NULL);
//Copy user data to the transmit buffer
netBufferRead((uint8_t *) CPPI_SWAP(txCurBufferDesc->word1), buffer,
offset, length);
//Set the length of the buffer
txCurBufferDesc->word2 = CPPI_SWAP(length & EMAC_TX_WORD2_BUFFER_LENGTH);
//Give the ownership of the descriptor to the DMA
txCurBufferDesc->word3 = CPPI_SWAP(EMAC_TX_WORD3_SOP | EMAC_TX_WORD3_EOP |
EMAC_TX_WORD3_OWNER | (length & EMAC_TX_WORD3_PACKET_LENGTH));
//Link the current descriptor to the previous descriptor
txCurBufferDesc->prev->word0 = CPPI_SWAP(txCurBufferDesc);
//Read the status flags of the previous descriptor
temp = CPPI_SWAP(txCurBufferDesc->prev->word3) & (EMAC_TX_WORD3_SOP |
EMAC_TX_WORD3_EOP | EMAC_TX_WORD3_OWNER | EMAC_TX_WORD3_EOQ);
//Misqueued buffer condition?
if(temp == (EMAC_TX_WORD3_SOP | EMAC_TX_WORD3_EOP | EMAC_TX_WORD3_EOQ))
{
//Clear the misqueued buffer condition
txCurBufferDesc->prev->word3 = CPPI_SWAP(0);
//The host corrects the misqueued buffer condition by writing the
//misqueued packet�s buffer descriptor address to the appropriate
//TX DMA head descriptor pointer
EMAC_TXHDP_R(EMAC_CH0) = (uint32_t) txCurBufferDesc;
}
//Point to the next descriptor in the list
txCurBufferDesc = txCurBufferDesc->next;
//Check whether the next buffer is available for writing
if((CPPI_SWAP(txCurBufferDesc->word3) & EMAC_TX_WORD3_OWNER) == 0)
{
//The transmitter can accept another packet
osSetEvent(&interface->nicTxEvent);
}
//Data successfully written
return NO_ERROR;
}
/**
* @brief Receive a packet
* @param[in] interface Underlying network interface
* @return Error code
**/
error_t tms570EthReceivePacket(NetInterface *interface)
{
static uint32_t buffer[TMS570_ETH_RX_BUFFER_SIZE / 4];
error_t error;
size_t n;
uint32_t temp;
//Current buffer available for reading?
if((CPPI_SWAP(rxCurBufferDesc->word3) & EMAC_RX_WORD3_OWNER) == 0)
{
//SOP and EOP flags should be set
if((CPPI_SWAP(rxCurBufferDesc->word3) & EMAC_RX_WORD3_SOP) != 0 &&
(CPPI_SWAP(rxCurBufferDesc->word3) & EMAC_RX_WORD3_EOP) != 0)
{
//Make sure no error occurred
if((CPPI_SWAP(rxCurBufferDesc->word3) & EMAC_RX_WORD3_ERROR_MASK) == 0)
{
//Retrieve the length of the frame
n = CPPI_SWAP(rxCurBufferDesc->word3) & EMAC_RX_WORD3_PACKET_LENGTH;
//Limit the number of data to read
n = MIN(n, TMS570_ETH_RX_BUFFER_SIZE);
//Copy data from the receive buffer
osMemcpy(buffer, (uint8_t *) CPPI_SWAP(rxCurBufferDesc->word1), n);
//Valid packet received
error = NO_ERROR;
}
else
{
//The received packet contains an error
error = ERROR_INVALID_PACKET;
}
}
else
{
//The packet is not valid
error = ERROR_INVALID_PACKET;
}
//Mark the end of the queue with a NULL pointer
rxCurBufferDesc->word0 = CPPI_SWAP(NULL);
//Restore the length of the buffer
rxCurBufferDesc->word2 = CPPI_SWAP(TMS570_ETH_RX_BUFFER_SIZE);
//Give the ownership of the descriptor back to the DMA
rxCurBufferDesc->word3 = CPPI_SWAP(EMAC_RX_WORD3_OWNER);
//Link the current descriptor to the previous descriptor
rxCurBufferDesc->prev->word0 = CPPI_SWAP(rxCurBufferDesc);
//Read the status flags of the previous descriptor
temp = CPPI_SWAP(rxCurBufferDesc->prev->word3) & (EMAC_RX_WORD3_SOP |
EMAC_RX_WORD3_EOP | EMAC_RX_WORD3_OWNER | EMAC_RX_WORD3_EOQ);
//Misqueued buffer condition?
if(temp == (EMAC_RX_WORD3_SOP | EMAC_RX_WORD3_EOP | EMAC_RX_WORD3_EOQ))
{
//The host acts on the misqueued buffer condition by writing the added
//buffer descriptor address to the appropriate RX DMA head descriptor
//pointer
EMAC_RXHDP_R(EMAC_CH0) = (uint32_t) rxCurBufferDesc;
}
//Write the RX completion pointer
EMAC_RXCP_R(EMAC_CH0) = (uint32_t) rxCurBufferDesc;
//Point to the next descriptor in the list
rxCurBufferDesc = rxCurBufferDesc->next;
}
else
{
//No more data in the receive buffer
error = ERROR_BUFFER_EMPTY;
}
//Check whether a valid packet has been received
if(!error)
{
NetRxAncillary ancillary;
//Additional options can be passed to the stack along with the packet
ancillary = NET_DEFAULT_RX_ANCILLARY;
//Pass the packet to the upper layer
nicProcessPacket(interface, (uint8_t *) buffer, n, &ancillary);
}
//Return status code
return error;
}
/**
* @brief Configure MAC address filtering
* @param[in] interface Underlying network interface
* @return Error code
**/
error_t tms570EthUpdateMacAddrFilter(NetInterface *interface)
{
uint_t i;
uint_t k;
uint8_t *p;
uint32_t hashTable[2];
MacFilterEntry *entry;
//Debug message
TRACE_DEBUG("Updating MAC filter...\r\n");
//Clear hash table
hashTable[0] = 0;
hashTable[1] = 0;
//The MAC address filter contains the list of MAC addresses to accept
//when receiving an Ethernet frame
for(i = 0; i < MAC_ADDR_FILTER_SIZE; i++)
{
//Point to the current entry
entry = &interface->macAddrFilter[i];
//Valid entry?
if(entry->refCount > 0)
{
//Point to the MAC address
p = entry->addr.b;
//Apply the hash function
k = (p[0] >> 2) ^ (p[0] << 4);
k ^= (p[1] >> 4) ^ (p[1] << 2);
k ^= (p[2] >> 6) ^ p[2];
k ^= (p[3] >> 2) ^ (p[3] << 4);
k ^= (p[4] >> 4) ^ (p[4] << 2);
k ^= (p[5] >> 6) ^ p[5];
//The hash value is reduced to a 6-bit index
k &= 0x3F;
//Update hash table contents
hashTable[k / 32] |= (1 << (k % 32));
}
}
//Write the hash table
EMAC_MACHASH1_R = hashTable[0];
EMAC_MACHASH2_R = hashTable[1];
//Debug message
TRACE_DEBUG(" MACHASH1 = %08" PRIX32 "\r\n", EMAC_MACHASH1_R);
TRACE_DEBUG(" MACHASH2 = %08" PRIX32 "\r\n", EMAC_MACHASH2_R);
//Successful processing
return NO_ERROR;
}
/**
* @brief Adjust MAC configuration parameters for proper operation
* @param[in] interface Underlying network interface
* @return Error code
**/
error_t tms570EthUpdateMacConfig(NetInterface *interface)
{
uint32_t config;
//Read MAC control register
config = EMAC_MACCONTROL_R;
//100BASE-TX or 10BASE-T operation mode?
if(interface->linkSpeed == NIC_LINK_SPEED_100MBPS)
{
config |= EMAC_MACCONTROL_RMIISPEED;
}
else
{
config &= ~EMAC_MACCONTROL_RMIISPEED;
}
//Half-duplex or full-duplex mode?
if(interface->duplexMode == NIC_FULL_DUPLEX_MODE)
{
config |= EMAC_MACCONTROL_FULLDUPLEX;
}
else
{
config &= ~EMAC_MACCONTROL_FULLDUPLEX;
}
//Update MAC control register
EMAC_MACCONTROL_R = config;
//Successful processing
return NO_ERROR;
}
/**
* @brief Write PHY register
* @param[in] opcode Access type (2 bits)
* @param[in] phyAddr PHY address (5 bits)
* @param[in] regAddr Register address (5 bits)
* @param[in] data Register value
**/
void tms570EthWritePhyReg(uint8_t opcode, uint8_t phyAddr,
uint8_t regAddr, uint16_t data)
{
uint32_t temp;
//Valid opcode?
if(opcode == SMI_OPCODE_WRITE)
{
//Set up a write operation
temp = MDIO_USERACCESS0_GO | MDIO_USERACCESS0_WRITE;
//PHY address
temp |= (phyAddr << MDIO_USERACCESS0_PHYADR_SHIFT) & MDIO_USERACCESS0_PHYADR;
//Register address
temp |= (regAddr << MDIO_USERACCESS0_REGADR_SHIFT) & MDIO_USERACCESS0_REGADR;
//Register value
temp |= data & MDIO_USERACCESS0_DATA;
//Start a write operation
MDIO_USERACCESS0_R = temp;
//Wait for the write to complete
while((MDIO_USERACCESS0_R & MDIO_USERACCESS0_GO) != 0)
{
}
}
else
{
//The MAC peripheral only supports standard Clause 22 opcodes
}
}
/**
* @brief Read PHY register
* @param[in] opcode Access type (2 bits)
* @param[in] phyAddr PHY address (5 bits)
* @param[in] regAddr Register address (5 bits)
* @return Register value
**/
uint16_t tms570EthReadPhyReg(uint8_t opcode, uint8_t phyAddr,
uint8_t regAddr)
{
uint16_t data;
uint32_t temp;
//Valid opcode?
if(opcode == SMI_OPCODE_READ)
{
//Set up a read operation
temp = MDIO_USERACCESS0_GO | MDIO_USERACCESS0_READ;
//PHY address
temp |= (phyAddr << MDIO_USERACCESS0_PHYADR_SHIFT) & MDIO_USERACCESS0_PHYADR;
//Register address
temp |= (regAddr << MDIO_USERACCESS0_REGADR_SHIFT) & MDIO_USERACCESS0_REGADR;
//Start a read operation
MDIO_USERACCESS0_R = temp;
//Wait for the read to complete
while((MDIO_USERACCESS0_R & MDIO_USERACCESS0_GO) != 0)
{
}
//Get register value
data = MDIO_USERACCESS0_R & MDIO_USERACCESS0_DATA;
}
else
{
//The MAC peripheral only supports standard Clause 22 opcodes
data = 0;
}
//Return the value of the PHY register
return data;
}
I need assistance converting our Ethernet driver for the TMS570LS1227 from the current implementation in tms570_eth_driver.c and tms570_eth_driver.h to the new APIs provided by HalCoGen in CCS.
Details:
- Current Files:
tms570_eth_driver.c,tms570_eth_driver.h - Target Platform: TMS570LS1227
- Current Driver: Used with CycloneTCP
Assistance Required:
- API Mapping: Help with mapping existing functions to HalCoGen APIs, including initialization, interrupt handling, and packet operations.
- Example Code: Any examples or guidelines for using the new APIs effectively.
- Documentation: Relevant references or documentation.
Thank you for your support.