Part Number: MSPM0G3507
Tool/software:
Hello TI expert,
When I play with LP_MSPM0G3507 launch pad on uart_callback_freertos_ticlang example. I encounter a problem and don't understand.
Why uart interrupt always get triggered? indeed TX and RX line are clean.
CCS Version: 12.7.1.00001
MSPM0 sdk version: mspm0_sdk_2_01_00_03
example: C:\ti\mspm0_sdk_2_01_00_03\examples\rtos\LP_MSPM0G3507\drivers\uart_echo
the code could be executed and echo function works well as below.

However, when I put a breakpoint at UART0_IRQHandler(void) function, it always get triggered. as shown below
seems like DMA related flag always being set.

then I put a breakpoint at xPortSysTickHandler(void). it never get triggered. seems like system tick preempted by UART interrupt.

How could explain this?