Part Number: LP-MSPM0L1306
Other Parts Discussed in Thread: MSPM0L1306
Tool/software:
Hi forum
I'm working on a project where I use the MSPM0L1306 launchpad and CCS to program and debug the launchpad, but i haven't gotten any places since, when i try to upload code to the launchpad it wants me to update the XDS110 to a new firmware_3.0.0.31 and when i press update it gives me this error
"CS_DAP_0: Error: (Error -591 @ 0x0) The firmware updater encountered an error and could not finish. The updater failed to connect to the XDS110 in programming mode. Unplug and re-plug the XDS110, and try again. If the problem remains, try updating the firmware using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of the installation. View the XDS110SupportReadMe.pdf file there for instructions. (Emulation package 12.8.0.00189)".
I also tried to do it in CMD and it can find the device but when the command "xdsdfu -m" is used to put it into DFU mode it loses all connections, and the drivers for the device under device manager becomes "Tiva Device Firmware update", so when i use the firmware update command it tells it cant find a device.
The current firmware that is on the XDS110 is 3.0.0.22
Code composer studio version 12.8.0.00012