Part Number: RM46L852
Other Parts Discussed in Thread: TMDXRM46HDK, SN74LV1T32, LAUNCHXL2-RM46
Tool/software:
Hi,
I believe that I have detected a mistake in the RM46L852 documentation. The following pictures show this mistake:
On page 1941 of User guide

On page 1942 of User guide

On page 23 of Datasheet

On page 17 of TMDXRM46HDK schematic

According to the documentation, it is necessary to add a signal level shifter (5 V -> 3.3 V) to avoid damaging the USB_VBUS pin. However, this recommendation it is not reflected in both schematics. So, I consider that there is a mistake. The 100 kohm resistor protects the pin of a high current, but I am not sure if a voltage of 3.3V can be obtained with this resistor. I would like to know your opinion about this, it is possible that I have misinterpretation all this.
Best regards,
Francisco.