Part Number: LP-AM263P
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hello,
I am using the gpio_input_interrupt_am263px-LP example and want to trigger an input interrupt using SPI1_CS0 or SPI0_D1.
I have changed only the settings for "GPIO PUSH BUTTON" as shown below.

In my test, I simply put 3.3V on pin J6.58 for SPI1_CS0, or J6.54 for SPI0_D1, but it won't trigger an interrupt.
I suspect the issue is XBAR. I have not changed the XBAR Input settings in sysconfig. Is this the issue? If so, how do I determine what settings XBAR should be for each input?
Best,
David