Part Number: MSPM0G1107
Other Parts Discussed in Thread: MSPM0G3507, , SYSCONFIG, LP-MSPM0G3507
Tool/software:
We're running some benchmarks and trying to determine why the task context switch seems relatively slow when trying to wake a task from an ISR (using a semaphore or FreeRTOS task notification). It's taking about 25 us with the CPU clock running at 80 MHz, which comes out to about 2000 CPU cycles. We were expecting the latency to be much faster. The task is set to the highest priority, We started with the mspm0_sdk_2_01_00_03\examples\rtos\LP_MSPM0G3507\kernel\posix_demo example and reconfigured it for an MSPM0G1107.
Here's the entirety of the UART task and ISR code:
/*
* Includes
*/
// Project-specific
#include "ti_msp_dl_config.h"
// Standard C library
#include <assert.h>
#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <string.h>
// RTOS header files
#include <FreeRTOS.h>
#include <portmacro.h>
#include <semphr.h>
// TI
#include <ti/drivers/dpl/HwiP.h>
/*
* Local variables
*/
static SemaphoreHandle_t m_semaphore;
volatile uint8_t v_rxByte;
/*
* Global functions
*/
void UART3_IRQHandler(void)
{
uint8_t rxByte;
switch(DL_UART_Main_getPendingInterrupt(UART_RS485_INST))
{
case DL_UART_IIDX_RX:
while(DL_UART_receiveDataCheck(UART_RS485_INST, &v_rxByte))
{
// Unloaded a byte.
}
// Signal the task to transmit.
xSemaphoreGiveFromISR(m_semaphore, &(BaseType_t) {});
break;
default:
break;
}
}
void *RS845_thread(void *arg0)
{
// Initialize semaphore to signal transmit operation.
m_semaphore = xSemaphoreCreateBinary();
/*
* Reconfigure UART.
*/
DL_UART_Main_disable(UART_RS485_INST);
DL_UART_clearInterruptStatus(UART_RS485_INST, -1);
// Enable UART interrupt in the NVIC.
HwiP_clearInterrupt(UART3_INT_IRQn);
HwiP_enableInterrupt(UART3_INT_IRQn);
/*
* End UART reconfiguration.
*/
DL_UART_Main_enable(UART_RS485_INST);
while(1)
{
// Wait for rx timeout.
xSemaphoreTake(m_semaphore, portMAX_DELAY);
// Transmit a character.
DL_UART_transmitDataBlocking(UART_RS485_INST, '$');
}
}
Here's a logic analyzer capture showing the latency between the received byte and the transmitted byte.

In main.c, the task stack size was increased and priority set to max:
diff --git a/main.c b/main.c
index 0f392b2..b1c096a 100644
--- a/main.c
+++ b/main.c
@@ -49,7 +49,7 @@
extern void *RS845_thread(void *arg0);
/* Stack size in bytes */
-#define THREADSTACKSIZE 256
+#define THREADSTACKSIZE 1024
/* Set up the hardware ready to run this demo */
static void prvSetupHardware(void);
@@ -73,8 +73,8 @@ int main(void)
pthread_attr_init(&attrs);
/* Set priority, detach state, and stack size attributes */
- priParam.sched_priority = 1;
- retc = pthread_attr_setschedparam(&attrs, &priParam);
+ priParam.sched_priority = configMAX_PRIORITIES - 1;
+ retc = pthread_attr_setschedparam(&attrs, &priParam);
retc |= pthread_attr_setdetachstate(&attrs, PTHREAD_CREATE_DETACHED);
retc |= pthread_attr_setstacksize(&attrs, THREADSTACKSIZE);
if (retc != 0) {
SysConfig setup:
/**
* These arguments were used when this file was generated. They will be automatically applied on subsequent loads
* via the GUI or CLI. Run CLI with '--help' for additional information on how to override these arguments.
* @cliArgs --device "MSPM0G110X" --part "Default" --package "VQFN-32(RHB)" --product "mspm0_sdk@2.01.00.03"
* @v2CliArgs --device "MSPM0G1107" --package "VQFN-32(RHB)" --product "mspm0_sdk@2.01.00.03"
* @versions {"tool":"1.21.1+3772"}
*/
/**
* Import the modules used in this configuration.
*/
const GPIO = scripting.addModule("/ti/driverlib/GPIO", {}, false);
const GPIO1 = GPIO.addInstance();
const SYSCTL = scripting.addModule("/ti/driverlib/SYSCTL");
const TIMER = scripting.addModule("/ti/driverlib/TIMER", {}, false);
const TIMER1 = TIMER.addInstance();
const UART = scripting.addModule("/ti/driverlib/UART", {}, false);
const UART1 = UART.addInstance();
const ProjectConfig = scripting.addModule("/ti/project_config/ProjectConfig");
/**
* Write custom configuration values to the imported modules.
*/
const divider6 = system.clockTree["PLL_CLK2X_DIV"];
divider6.divideValue = 5;
const divider9 = system.clockTree["UDIV"];
divider9.divideValue = 2;
const multiplier2 = system.clockTree["PLL_QDIV"];
multiplier2.multiplyValue = 8;
const mux4 = system.clockTree["EXHFMUX"];
mux4.inputSelect = "EXHFMUX_XTAL";
const mux8 = system.clockTree["HSCLKMUX"];
mux8.inputSelect = "HSCLKMUX_SYSPLL2X";
const mux12 = system.clockTree["SYSPLLMUX"];
mux12.inputSelect = "zSYSPLLMUX_HFCLK";
const oscillator2 = system.clockTree["SYSOSC"];
oscillator2.enableSYSOSCFCL = true;
const pinFunction4 = system.clockTree["HFXT"];
pinFunction4.inputFreq = 25;
pinFunction4.enable = true;
GPIO1.$name = "GPIO_RS485";
GPIO1.port = "PORTA";
GPIO1.associatedPins.create(3);
GPIO1.associatedPins[0].initialValue = "SET";
GPIO1.associatedPins[0].ioStructure = "SD";
GPIO1.associatedPins[0].$name = "PIN_RS485_TX_EN";
GPIO1.associatedPins[0].pin.$assign = "PA27";
GPIO1.associatedPins[1].$name = "PIN_RS485_RX_EN";
GPIO1.associatedPins[1].pin.$assign = "PA0";
GPIO1.associatedPins[2].$name = "PIN_RS485_TERM_EN";
GPIO1.associatedPins[2].initialValue = "SET";
GPIO1.associatedPins[2].pin.$assign = "PA1";
const Board = scripting.addModule("/ti/driverlib/Board", {}, false);
Board.peripheral.$assign = "DEBUGSS";
Board.peripheral.swclkPin.$assign = "PA20";
Board.peripheral.swdioPin.$assign = "PA19";
SYSCTL.HFCLKSource = "HFXT";
SYSCTL.HFCLK_Freq = 25000000;
SYSCTL.enableSYSOSCFCL = true;
SYSCTL.SYSPLL_Pdiv = 4;
SYSCTL.SYSPLL_Qdiv = 5;
SYSCTL.SYSPLL_CLK2XEn = true;
SYSCTL.clockTreeEn = true;
SYSCTL.validateClkStatus = true;
TIMER1.timerClkDiv = 8;
TIMER1.interrupts = ["ZERO"];
TIMER1.$name = "TIMER_RS485_RESPONSE";
UART1.$name = "UART_RS485";
UART1.ovsRate = "8";
UART1.targetBaudRate = 8000000;
UART1.rxFifoThreshold = "DL_UART_RX_FIFO_LEVEL_ONE_ENTRY";
UART1.interruptPriority = "1";
UART1.enabledInterrupts = ["RX"];
UART1.peripheral.$assign = "UART3";
UART1.peripheral.rxPin.$assign = "PA25";
UART1.peripheral.txPin.$assign = "PA26";
UART1.txPinConfig.$name = "ti_driverlib_gpio_GPIOPinGeneric0";
UART1.txPinConfig.direction = scripting.forceWrite("OUTPUT");
UART1.txPinConfig.hideOutputInversion = scripting.forceWrite(false);
UART1.txPinConfig.onlyInternalResistor = scripting.forceWrite(false);
UART1.txPinConfig.passedPeripheralType = scripting.forceWrite("Digital");
UART1.txPinConfig.enableConfig = true;
UART1.rxPinConfig.$name = "ti_driverlib_gpio_GPIOPinGeneric1";
UART1.rxPinConfig.hideOutputInversion = scripting.forceWrite(false);
UART1.rxPinConfig.onlyInternalResistor = scripting.forceWrite(false);
UART1.rxPinConfig.passedPeripheralType = scripting.forceWrite("Digital");
ProjectConfig.genDisable = true;
ProjectConfig.deviceSpin = "MSPM0G1107";
/**
* Pinmux solution for unlocked pins/peripherals. This ensures that minor changes to the automatic solver in a future
* version of the tool will not impact the pinmux you originally saw. These lines can be completely deleted in order to
* re-solve from scratch.
*/
pinFunction4.peripheral.$suggestSolution = "SYSCTL";
pinFunction4.peripheral.hfxInPin.$suggestSolution = "PA5";
pinFunction4.peripheral.hfxOutPin.$suggestSolution = "PA6";
TIMER1.peripheral.$suggestSolution = "TIMA0";
FreeRTOSConfig.h file is mostly unmodified from the example. Only the CPU clock was adjusted:
diff --git a/FreeRTOSConfig.h b/FreeRTOSConfig.h index 20e4040..b5e2ac5 100644 --- a/FreeRTOSConfig.h +++ b/FreeRTOSConfig.h @@ -70,7 +70,7 @@ #define configUSE_16_BIT_TICKS 0 /* Only for 8 and 16-bit hardware. */ /* Constants that describe the hardware and memory usage. */ -#define configCPU_CLOCK_HZ ((unsigned long) 32000000) +#define configCPU_CLOCK_HZ ((unsigned long) 80000000) /* Smallest stack size allowed in words */ #define configMINIMAL_STACK_SIZE ((unsigned short) 128) #define configMAX_TASK_NAME_LEN (12)