Part Number: TM4C1294NCPDT
Tool/software:
I need to add more external flash to a TM4C1294NCPDT CPU. I assume the best way to do this is by using the USB or SPI interface but if there is something better let me know. Most flash devices support SPI and I think some can use USB. I don't need a file system because we just need to "stream" some large amount of data in and out of flash via Ethernet.
If the flash memory size needed is 1 GigBit, what memory would be recommended and what is the best performance that could be expected?
The project uses TM4C1294NCPDT, CCS 8.3.0, TIRTOS 2.16.1.14.
Thanks,
Doug