Part Number: TMS570LS1227
Other Parts Discussed in Thread: HALCOGEN
Tool/software:
The sys_selftest.c generated by HalCoGen contains this function:
boolean pbistIsTestCompleted(void)
{
return ((systemREG1->MSTCGSTAT & 0x1U) != 0U);
}It violates MISRA-C 2004 12.2 "Volatile variable in complex expression", so I replace it by this equivalent function
boolean pbistIsTestCompleted(void)
{
uint32 stat = systemREG1->MSTCGSTAT;
return ((stat & 0x1U) != 0U);
}
After this modification, the system goes into prefetch abort exception. nError pin seems to go wild that a relay controlled by that pin switches back and forth.
The registers are CP15.IFSR=0x0d, CP15.IFAR=0xc3c3c3c2 (an invalid address), CP15.AIFSR=0x0.
If I undo this modification, the prefetch abort disappears. If I add it back, the prefetch happens again. If I run the code in debugger step by step, the prefetch disappears.
I think it isn't my code that causes this problem because it goes to prefetch exception before running main(), and the code runs before main() is generated by HalCoGen, except pbistIsTestCompleted.
Although the C code seems equivalent, the assembly is quite different. But I can't see why it has anything to do with prefetch abort. Compiler flags are -mv7R4 --code_state=32 --float_support=VFPv3D16 --include_path="C:/ti/ccs1260/ccs/tools/compiler/ti-cgt-arm_20.2.7.LTS/include" --include_path="C:/ti/Hercules/F021 Flash API/02.01.01/include" -g --symdebug:dwarf_version=3 --c99 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --gen_data_subsections=on --enum_type=packed --abi=eabi.
boolean pbistIsTestCompleted(void)
{
return ((systemREG1->MSTCGSTAT & 0x1U) != 0U);
}
pbistIsTestCompleted():
000176cc: E3E0C097 mvn r12, #0x97
000176d0: E59C1000 ldr r1, [r12]
000176d4: E3A00000 mov r0, #0
000176d8: E3110001 tst r1, #1
000176dc: E3A0C000 mov r12, #0
000176e0: 0A000000 beq $C$L11
000176e4: E3A0C001 mov r12, #1
$C$L11:
000176e8: E35C0000 cmp r12, #0
000176ec: 0A000000 beq $C$L12
000176f0: E3A00001 mov r0, #1
315 }
$C$L12:
000176f4: E12FFF1E bx lr
boolean pbistIsTestCompleted(void)
{
uint32 stat = systemREG1->MSTCGSTAT;
return ((stat & 0x1U) != 0U);
}
pbistIsTestCompleted():
00016ea0: E24DD008 sub r13, r13, #8
312 uint32 stat = systemREG1->MSTCGSTAT;
00016ea4: E3E0C097 mvn r12, #0x97
00016ea8: E59CC000 ldr r12, [r12]
00016eac: E58DC000 str r12, [r13]
313 return ((stat & 0x1U) != 0U);
00016eb0: E59D1000 ldr r1, [r13]
00016eb4: E3A00000 mov r0, #0
00016eb8: E3110001 tst r1, #1
00016ebc: E3A0C000 mov r12, #0
00016ec0: 0A000000 beq $C$L11
00016ec4: E3A0C001 mov r12, #1
$C$L11:
00016ec8: E35C0000 cmp r12, #0
00016ecc: 0A000000 beq $C$L12
00016ed0: E3A00001 mov r0, #1
316 }
$C$L12:
00016ed4: E28DD008 add r13, r13, #8
00016ed8: E12FFF1E bx lr
Why does this happen? How can I locate the problem? Thanks very much!