Tool/software:
Hello,
I am trying to perform an analog loopback test for the LIN module using the SafeTI Diagnostic Library. When I call the function SL_SelfTest_LIN() for this purpose, it fails at the step where it verifies if the LIN module is out of the reset state. The return value retVal is set to FALSE. Here's the code snippet that performs the reset state check:
status = SL_SelfTest_LIN(LIN_ANALOG_LOOPBACK_TEST, SL_LIN1);
/*verify LIN is not in reset state */
/*SAFETYMCUSW 439 S MR:11.3 <APPROVED> Comment_4*/
if(sl_linREG != NULL)
{
/*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_5*/
if((LIN_GCR0_RESET_BIT|LIN_GCR1_SWRST_BIT) != (sl_linREG->GCR0 & (LIN_GCR0_RESET_BIT|LIN_GCR1_SWRST_BIT)))
{
#if (FUNC_ENTRY_COND_CHECK_LOG_ENABLED !=0)
SL_Log_Error(FUNC_ID_ST_LIN, ERR_TYPE_ENTRY_CON, 1u);
#endif
retVal = FALSE;
return retVal;
}
As I understand, this condition checks if sl_linREG->GCR0 has the value 0x81. However, the GCR0 register, cannot have this value, which makes me wonder if this is a bug in the SafeTI Diagnostic Library.
Here is my initialization function for LIN module
void sciInit(UartInit_t* Uart_init_struct)
{
/* USER CODE BEGIN (2) */
/* USER CODE END */
/** @b initialize @b SCILIN */
/** - bring SCI out of reset */
scilinREG->GCR0 = 0U;
scilinREG->GCR0 = 1U;
/** - Disable all interrupts */
scilinREG->CLEARINT = 0xFFFFFFFFU;
scilinREG->CLEARINTLVL = 0xFFFFFFFFU;
/** - global control 1 */
scilinREG->GCR1 = (uint32)((uint32)1U << 25U) /* enable transmit */
| (uint32)((uint32)1U << 24U) /* enable receive */
| (uint32)((uint32)1U << 5U) /* internal clock (device has no clock pin) */
| (uint32)((uint32)(Uart_init_struct->stop_bits-1U) << 4U) /* number of stop bits */
| (uint32)((uint32)Uart_init_struct->parity_even << 3U) /* even parity, otherwise odd */
| (uint32)((uint32)Uart_init_struct->parity_enable << 2U) /* enable parity */
| (uint32)((uint32)1U << 1U); /* asynchronous timing mode */
/** - set baudrate */
sciSetBaudrate(scilinREG,(uint32) Uart_init_struct->baud_rate );
/** - transmission length */
scilinREG->FORMAT = 8U - 1U; /* length */
/** - set SCI pins functional mode */
scilinREG->PIO0 = (uint32)((uint32)1U << 2U) /* tx pin */
| (uint32)((uint32)1U << 1U); /* rx pin */
/** - set SCI pins default output value */
scilinREG->PIO3 = (uint32)((uint32)0U << 2U) /* tx pin */
| (uint32)((uint32)0U << 1U); /* rx pin */
/** - set SCI pins output direction */
scilinREG->PIO1 = (uint32)((uint32)0U << 2U) /* tx pin */
| (uint32)((uint32)0U << 1U); /* rx pin */
/** - set SCI pins open drain enable */
scilinREG->PIO6 = (uint32)((uint32)0U << 2U) /* tx pin */
| (uint32)((uint32)0U << 1U); /* rx pin */
/** - set SCI pins pullup/pulldown enable */
scilinREG->PIO7 = (uint32)((uint32)0U << 2U) /* tx pin */
| (uint32)((uint32)0U << 1U); /* rx pin */
/** - set SCI pins pullup/pulldown select */
scilinREG->PIO8 = (uint32)((uint32)1U << 2U) /* tx pin */
| (uint32)((uint32)1U << 1U); /* rx pin */
/** - set interrupt level */
scilinREG->SETINTLVL = (uint32)((uint32)0U << 26U) /* Framing error */
| (uint32)((uint32)0U << 25U) /* Overrun error */
| (uint32)((uint32)0U << 24U) /* Parity error */
| (uint32)((uint32)0U << 9U) /* Receive */
| (uint32)((uint32)0U << 8U) /* Transmit */
| (uint32)((uint32)0U << 1U) /* Wakeup */
| (uint32)((uint32)0U); /* Break detect */
/** - set interrupt enable */
scilinREG->SETINT = (uint32)((uint32)0U << 26U) /* Framing error */
| (uint32)((uint32)0U << 25U) /* Overrun error */
| (uint32)((uint32)0U << 24U) /* Parity error */
| (uint32)((uint32)1U << 9U) /* Receive */
| (uint32)((uint32)0U << 1U) /* Wakeup */
| (uint32)((uint32)0U); /* Break detect */
/** - initialize global transfer variables */
g_sciTransfer_t[1U].mode = (uint32)1U << 8U;
g_sciTransfer_t[1U].tx_length = 0U;
g_sciTransfer_t[1U].rx_length = 0U;
/** - Finaly start SCILIN */
scilinREG->GCR1 |= 0x80U;
/* USER CODE BEGIN (3) */
/* USER CODE END */
}
GCR0 register is set to 1, which means that module is out of reset, and at the end GCR1 is set to 0x80.

Is this a software bug in the library, or is there a configuration issue on my side?
Thanks & regards,
Ilija