Part Number: MSPM0L2228
Tool/software:
Hi Team ,
I am using the internal Flash memory of the MSPM0L2228 to store the data.
Initially i am able to store the data in the internal Flash memory of the controller. but after some time the data that i stored not able to get it back, memory get erased.
there are two cases on which internal memory get erased,
1. when the controller get heated.
2. when multiple times device on off .
Is there is any provision that i have to follow,
Or any other protection to store the data in Flash memory, which i can get my data back after stored.
Thank you,
Ankush