Part Number: AM263P4
Tool/software:
Hi,
To make the Fls works with Autosar Fee module, I have to do some changes in Fls driver.
in function Fls_Ospi_readDirect:
pSrc = (uint8 *)(FLS_BASE_ADDRESS + addrOffset);
#if 0
remainSize = (uint32)trans->count & 3U;
size = (uint32)trans->count - remainSize;
/* Transfer the data in 32-bit size */
for (i = 0U; i < size; i += 4U)
{
HW_WR_REG32(pDst + i, HW_RD_REG32(pSrc + i));
}
/* Transfer the remaining data in 8-bit size */
for (i = 0; i < remainSize; i++)
{
HW_WR_REG32(pDst + size + i, HW_RD_REG8(pSrc + size + i));
}
#endif
/* This code is used to replace the comment out code above
to avoid data abort exception which cased by alignment issue
at function HW_WR_REG32(). 12/2024 by Phoenix
*/
for (i = 0; i < trans->count; i++)
{
HW_WR_REG32(pDst + i, HW_RD_REG8(pSrc + i));
}
The other one is that I need to clear the register that was set by RBL.
HW_WR_FIELD32(FLS_OSPI_CTRL_BASE_ADDR + OSPI_DEV_INSTR_RD_CONFIG_REG, OSPI_DEV_INSTR_RD_CONFIG_REG_DUMMY_RD_CLK_CYCLES_FLD, 0);
Otherwise, I have to configure dummy cycle to 8 which may not necessary for us.
Please include those fix in the next mcal release.
thanks