This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
I have a question about the UNIFLASH tool.
We're using the launchpad board, and I'm using the guide
AM243x MCU+ SDK: Flashing Tools
as a template for flashing the application.
I have changed the config file to my needs, and I can use successfully the python command:
python uart_uniflash.py -p {name of your UART com port} --cfg={path to your edited config file}
After the board is switched from UART_BOOT_MODE to QSPI_BOOT, the application starts successfully.
I now want to use the TI Uniflash tool. The board is scanned, but flashing in UART_BOOT_MODE is not possible.
What am I doing wrong?
Best regards
Alexander
Hi,
If the flashing is already done, then what do you need the UNIFLASH tool for?
If you have already flashed via the python uart uniflash command, then there would be no further use of UART Uniflash tool, as the UART Uniflash tool serves an alternate to flashing via the commands.
Regards,
Vaibhav
Hi Vaibhav,
that's right from a technical point of view.
We are currently evaluating the use of the Sitata AM243 in our company.
In development, the developer is welcome to flash the board via python script. No problem.
This is not usable in production. Here is the use of the graphical flash tool a basic requirement.
So it is necessary for me to get this tool working.
Greetings
Alexander
Hi,
I am trying to flash this on the AM243-LP TI EVM and will update in sometime when I have further steps to talk about.
Regards,
Vaibhav
Hi,
I have been able to successfully flash via the Tool on AM243-LP TI EVM.
I followed the following steps:
Post this, I simply upload the SBL image, the application image and the XIP image and the flashing is seen to be successful.
Hope the above steps help.
Regards,
Vaibhav
Hallo Vaihav,
Thanks for testing.
After I manually switched the connection to serial, it works.
Do you have any idea why auto detect doesn't work?
Regards,
Alexander
Do you have any idea why auto detect doesn't work?
It is because, the autodetect just rightly selects the SoC/TI EVM and then in the next step which is where we choose device under New Configuration, we need to correctly select how we want to flash the data, either via JTAG or the Serial option.
Hope this helps you out.
Marking the thread closed.
Regards,
Vaibhav