Part Number: LP-AM243
Other Parts Discussed in Thread: MCU-PLUS-SDK-AM243X, UNIFLASH
Tool/software:
Hello.
My development environment is as follows
Environment:
CCS 12.7.0
MCU-PLUS-SDK-AM243X 10.01.00.32
LP-AM2434
I get an error when I start the ipc echo sample with SBL OSPI MULTI-PARTITION.
Starting OSPI Multi-Partition Bootloader ...
DMSC Firmware Version 10.0.8--v10.00.08 (Fiery Fox)
DMSC Firmware revision 0xa
DMSC ABI revision 4.0
Some tests have failed!!
SBL OSPI terminates normally.
DMSC Firmware Version 10.0.8--v10.00.08 (Fiery Fox)
DMSC Firmware revision 0xa
DMSC ABI revision 4.0
KPI_DATA: [BOOTLOADER_PROFILE] Boot Media : NOR SPI FLASH
KPI_DATA: [BOOTLOADER_PROFILE] Boot Media Clock : 100.000 MHz
KPI_DATA: [BOOTLOADER_PROFILE] Boot Image Size : 229 KB
KPI_DATA: [BOOTLOADER_PROFILE] Cores present :
m4f0-0
r5f1-0
r5f1-1
r5f0-0
r5f0-1
KPI_DATA: [BOOTLOADER PROFILE] SYSFW init : 11098us
KPI_DATA: [BOOTLOADER PROFILE] System_init : 11712us
KPI_DATA: [BOOTLOADER PROFILE] Drivers_open : 1636us
KPI_DATA: [BOOTLOADER PROFILE] Board_driversOpen : 478616us
KPI_DATA: [BOOTLOADER PROFILE] Sciclient Get Version : 9843us
KPI_DATA: [BOOTLOADER PROFILE] CPU load : 33050us
KPI_DATA: [BOOTLOADER PROFILE] SBL End : 2us
KPI_DATA: [BOOTLOADER_PROFILE] SBL Total Time Taken : 545961us
Image loading done, switching to application ...
[IPC NOTIFY ECHO] Message exchange started by main core !!!
[m4f0-0] 0.004038s : [IPC NOTIFY ECHO] Remote Core waiting for messages from main core ... !!!
[r5f0-1] 0.002116s : [IPC NOTIFY ECHO] Remote Core waiting for messages from main core ... !!!
[r5f0-1] 4.398251s : [IPC NOTIFY ECHO] Remote core has echoed all messages !!!
[r5f1-0] 0.003187s : [IPC NOTIFY ECHO] Remote Core waiting for messages from main core ... !!!
[r5f1-0] 4.399828s : [IPC NOTIFY ECHO] Remote core has echoed all messages !!!
[r5f1-1] 0.002506s : [IPC NOTIFY ECHO] Remote Core waiting for messages from main core ... !!!
[r5f1-1] 4.399405s : [IPC NOTIFY ECHO] Remote core has echoed all messages !!!
[IPC NOTIFY ECHO] All echoed messages received by main core from 4 remote cores !!!
[IPC NOTIFY ECHO] Messages sent to each core = 1000000
[IPC NOTIFY ECHO] Number of remote cores = 4
All tests have passed!!
[m4f0-0] 6.632182s : [IPC NOTIFY ECHO] Remote core has echoed all messages !!!
Is this a problem with the SBL?
Or is the LP2434 faulty?
Flash erase Command:
10.01.00.32: Flash Erase also fails.
09.02.01.05: Flash Erase succeeds.
cd C:\ti_am243x09020105\mcu_plus_sdk_am243x_10_01_00_32\tools\boot
python .\uart_uniflash.py --flash-writer=sbl_prebuilt\am243x-lp\sbl_uart_uniflash.release.hs_fs.tiimage -p COM9 --operation=erase --flash-offset=0 --erase-size=0x180000
PS C:\ti_am243x09020105\mcu_plus_sdk_am243x_10_01_00_32\tools\boot> python .\uart_uniflash.py --flash-writer=sbl_prebuilt\am243x-lp\sbl_uart_uniflash.release.hs_fs.tiimage -p COM9 --operation=erase --flash-offset=0 --erase-size=0x180000
Found flash writer ... sending sbl_prebuilt\am243x-lp\sbl_uart_uniflash.release.hs_fs.tiimage
Sent flashwriter sbl_prebuilt\am243x-lp\sbl_uart_uniflash.release.hs_fs.tiimage of size 308654 bytes in 29.31s.
Traceback (most recent call last):
File "C:\ti_am243x09020105\mcu_plus_sdk_am243x_10_01_00_32\tools\boot\uart_uniflash.py", line 770, in <module>
main(sys.argv[1:])
File "C:\ti_am243x09020105\mcu_plus_sdk_am243x_10_01_00_32\tools\boot\uart_uniflash.py", line 518, in main
elif linecfg.optype in ["flash-mcelf-xip"]:
^^^^^^^
UnboundLocalError: cannot access local variable 'linecfg' where it is not associated with a value
PS C:\ti_am243x09020105\mcu_plus_sdk_am243x_10_01_00_32\tools\boot>
Regards,
Yoshiki