Part Number: XDS110ISO-EVM
Hello,
We are planning to use XDS110 debug Probe for debugging our prototype PCBs. So, I need to install a 5-pin connector on our PCB, which will be connected to the XDS110 using a cable-connector assembly for 20 pin connector. I have reviewed the User's Guide, but it does not give specs for the connectors. It only states (page 8):
The CTI20 connector is a 20 pin IDC connector using .050 by .100 inch pitch.
1) Above info is confusing or may be wrong. The connector is a 20-pin 2 rows (10 pins/row) connector. I have looked at the photos of the 20 pin connector on XDS110 probe. It appears to be a 2.54mm (0.1 inch) pitch (center to center of pins), and 2.54mm row to row distance. So what is .050 ? (1.27mm).
2) Further on page 9, the User Guide states:
The AUX connection is a 14 pin IDC connection using .05 inch pitch.
Here, the guide does not state the second item ".100", which should define the row to row distance. But in the photos of the probe, this connector looks identical to the CTI20 (2 rows), except it has 14 pins.
3) I understand the two cables will come as part of the kit (20 pin and 14 pin) as shown in your website. So, what type of connector is on the other side of the cable? Male or female?
4) What AWG # wires are/can be used with these connectors? We will need to build our own 20 pin to 5 pin cable connector assemblies for different ptototype PCBs for testing using SWD interface.
Thanks.
AB