Part Number: AM263P4
Hi, I am using a AM263P and all the 4 cores. On core 1 I am using MCAN, and a bare metal OS.
The issue is the following, using 3 scenarios:
1.After running and uploading the SW, after some random time core 1 and 3 randomly disconects.
2.If I am flashing each core and not run them after some time core 1 and 3 randomly disconects.
3.If i just press connect target without loading the SW core 3 and 1 randomly disconects.
Cortex_R5_3: Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 21.0.0.3955)
Cortex_R5_3: Unable to determine target status after 20 attempts
Cortex_R5_3: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
Cortex_R5_1: Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 21.0.0.3955)
Cortex_R5_1: Unable to determine target status after 20 attempts
Cortex_R5_1: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging