This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2434: NOR Flash booting issue on custom board

Part Number: AM2434
Other Parts Discussed in Thread: SYSCONFIG

On our custom board we have AM2434ALV controller and S25HL512T NOR Flash,we have tried configuring NOR Flash with the TI SDK provided json file for S25HL512T in Sysconfig.
We ran the OSPI diagnostic program and we got the correct device ID and manufacturer ID and SFDP.Then we loaded uart example program through uart flashing using the ospi.cfg file.
we modified configuration of the flashwriter and bootloader according to our flash part number by uploading the json file.We were able to load the uart example along with bootloader and flashwriter 3 times then the 4th time,we were not able to flash the code.For the bootloader and flashwriter we used 4s-4d-4d protocol everytime.
The flashing stopped at --operation=flash-phy-tuning-data and the bootloader and app images were not flashing. Only the flashwriter of the cfg file was flashed.We replaced the NOR flash with new NOR Flash IC of same part number,but in that we were able to flash only once.
In the 2nd replaced NOR flash,after we flashed and changed to ospi boot mode,we were able to get the output.Then after one power cycle we tried checking the output,it didnt work.Further code flashing wasnt happening.
So we tried running the ospi flash diagnostic program,after they went to non working state,we got wrong device ID and manufacturer ID and no SFDP.We got Manufacturer ID as 0x9A and device ID is 0x150D.
But initially when we ran the the diagnostic program,it showed 0x34 and 0x2A1A.We have 2 custom boards,on one board we are able to get the IDs with adjusting dummy bit to 1 but no SFDP and all read write erase tests failed.
On another board we are not able to get IDs even with dummy bits=1,but erase is done and no SFDP with the same diagnostic code.Why is it working only two to three times initially and failing to boot or load the code?