Other Parts Discussed in Thread: HALCOGEN
Hi Chuck,
I am now looking at PBIST and specifically the initialisation of RAMs.
I am a little confused about the mapping of RAM groups to the MSIENA register. Does RAM group 1 map to bit 1 or bit 0 in MSIENA? is it the RAM group that I should be looking at in table 2-7 or RGS?
In startup code for the TMS570LS20x generated from Halcogen the value loaded to this register is 0x657F. Can you confirm exactly which memories this is enabling for initialisation/PBIST for this device?
Also, I am using the MibSPI modules in compatibility mode. Is PBIST of MibSPI RAM necessary when using this mode? Also, will setting the bit corresponding to MibSPI RAM in the MSIENA register cause initialisation to hang if MibSPI modules have not been released from reset?
Thanks,
Mark.