This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Tiva C Series TM4C1294 Connected LaunchPad



How can i connect the launchpad via ethernet with a hostname like http://MyLaunchpad.html instead an ip using lwip or uip

Best regards to all

  • From where?

    On a windows PC (or a linux desktop) there is a HOSTS file -- which I use.

    something like....

    192.168.0.11    hrsvr          # Hot Rocks server

    or from the example:

    #      102.54.94.97     rhino.acme.com          # source server

  • I should also mention that you can run DNS software if you have a unit on which you can run the software.

    That is a bit more complicated -- so I recommend using the HOST file on a PC that will be connecting to the launchpad unless you have a good reason to run a a DNS server -- on a Linux server is easiest to run the DNS daemon.

  • Hy Dave Thank You for Your Quick respond

    for my Application I need to connect the processor with a hostname because the IP will be unknown in most cases (DHCP) for example my Network Printer can be accessed with typing its name in Browsers navigation Bar how can i do this with connected launchpad ???

    Best Regards to all

  • Then you will need a DNS server (preferred) or a network with "permanently" fixed addresses -- take your pick.

    Since you want to use DHCP and descriptive names -- that means that you will have to set up a DNS server -- or register each piece of hardware with the ICANN registry -- or whatever-- don't see a way out of that.

    If this is an internal network -- or a client network that you control -- set up a DNS server then point each device to your DNS and DHCP server -- then let the server do the work.

    Without knowing your actual desired net configuration it's hard to give more advice.

  • It is also worth mentioning that the Video and course-ware refers to Exosite -- which provides the Gateway, DNS and DHCP service.

    http://www.ti.com/general/docs/video/Portal.tsp?entryid=0_1qe8j32e&lang=en%20%20%20

    If you have not looked at the Launchpad course-ware I can recommend it to explain these issues.

    Wiki and Courseware here:

    http://processors.wiki.ti.com/index.php/Creating_IoT_Solutions_with_the_TM4C1294XL_Connected_LaunchPad_Workshop?DCMP=tivac-launchpad&HQS=ConnectedLaunchPadWorkshop

    hth