This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC Digital Comparator working in Rising Edge mode but not Falling edge mode



I'm using Seq 0 for sampling data on both ADC's AIN2 on ADC0 and AIN3 on ADC1

Seq 1 is configured for generating Interrupt using Digital Comparator 0, Although both ADC are initialized only one ADC Seq 1 is enabled for interrupt generation when required

When I configure the DC for CIC = HIGH and CIM HONCE the interrupt generation happens properly at rising edge.

But when I configure DC for CIC = LOW and CIM = HONCE the interrupt is generated the moment I enable the Seq1. Is there anything wrong in the sequence of configuring/enabling various blocks

As Errata ADC#3 does not apply to TRIGGER_ALWAYS a single step has been configured.; works fine for rising edge.

****** extract from my program code

****** initialization

// Use ADC0 & ADC1 SEQ0 for Analog Channel Sampling
ROM_ADCSequenceConfigure(ADC0_BASE, 0, ADC_TRIGGER_TIMER, 0); // seq:0, priority:0
ROM_ADCSequenceConfigure(ADC1_BASE, 0, ADC_TRIGGER_TIMER, 0); // seq:0, priority:0

// Use ADC0 & ADC1 SEQ1 for Digital Comparator TRIGGER
ROM_ADCSequenceConfigure(ADC0_BASE, 1, ADC_TRIGGER_ALWAYS, 1); // seq:1, priority:1
ROM_ADCSequenceConfigure(ADC1_BASE, 1, ADC_TRIGGER_ALWAYS, 1); // seq:1, priority:1

ROM_ADCSequenceStepConfigure(ADC0_BASE,0,0,ADC_CTL_CH2|ADC_CTL_IE|ADC_CTL_END); // 
ROM_ADCSequenceStepConfigure(ADC1_BASE,0,0,ADC_CTL_CH3|ADC_CTL_IE|ADC_CTL_END);

ROM_ADCSequenceStepConfigure(ADC0_BASE,1,0,ADC_CTL_CH2|ADC_CTL_CMP0|ADC_CTL_END);
ROM_ADCSequenceStepConfigure(ADC1_BASE,1,0,ADC_CTL_CH3|ADC_CTL_CMP0|ADC_CTL_END);

********** run time config steps

ROM_ADCComparatorRegionSet(myTrigSrc, 0, myLevel, myLevel+0x80);

ROM_TimerLoadSet(WTIMER5_BASE,TIMER_A, (SYS_CLK_FREQ/myFreq) - 1);
ROM_TimerControlTrigger(WTIMER5_BASE,TIMER_A, true);

ROM_ADCSequenceEnable(ADC0_BASE, 0); // for sampling
ROM_ADCSequenceEnable(ADC1_BASE, 0);
ROM_ADCIntClear(ADC0_BASE, 0);
ROM_ADCIntEnable(ADC0_BASE, 0); // seq 0 uDMA intr enable
ROM_ADCIntClear(ADC1_BASE, 0);
ROM_ADCIntEnable(ADC1_BASE, 0);
// delay comparator
ROM_TimerEnable(WTIMER5_BASE,TIMER_A); // Sample Rate Timer Starts

******** some delay to fill sampled data before enabling Comparator (myTrigSrc is ADCx_BASE)********

if (AnalogTrigConfig & ALOG_TrigEdge) {
if (AnalogTrigConfig & ALOG_TrigLevel) { // Edge Mode
myTrig = ADC_COMP_INT_HIGH_HONCE;
} else {
myTrig = ADC_COMP_INT_LOW_HONCE;
}
} else {
if (AnalogTrigConfig & ALOG_TrigLevel) { // Level Mode
myTrig = ADC_COMP_INT_HIGH_ALWAYS;
} else {
myTrig = ADC_COMP_INT_LOW_ALWAYS;
}
}

ROM_ADCComparatorRegionSet(myTrigSrc, 0, myLevel, myLevel+0x80);
ROM_ADCComparatorConfigure(myTrigSrc, 0, myTrig );

ROM_ADCComparatorReset(myTrigSrc, 0, true, true);
ROM_ADCComparatorIntClear(myTrigSrc, ROM_ADCComparatorIntStatus(myTrigSrc));
ROM_ADCIntClear(myTrigSrc, 1);
ROM_ADCComparatorIntEnable(myTrigSrc, 1);
ROM_ADCIntEnable(myTrigSrc, 1);
ROM_ADCSequenceEnable(myTrigSrc, 1);