This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

need 0 to 100 % pwm generation on tiva 123g development board



Hi 

I am trying to generate a pwm signal of 25khz period.  and 0 to 100% duty cycle variation.  But i do not see 0-100% variation in pwm duty cycle.  the duty cycle and pulse width count relation is 0% -  170 ,  66% - for 400 and above. 

Below is the code.  I have used the code from the example.. I change the pulse width count manually for now.

void main(void)

{
 
uint32_t period;
 
 
 
//
    // Set the clocking to run directly from the external crystal/oscillator.
    // TODO: The SYSCTL_XTAL_ value must be changed to match the value of the
    // crystal on your board.
    //
 SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |
                SYSCTL_XTAL_16MHZ);
 
//SysCtlClockSet(SYSCTL_SYSDIV_16 | SYSCTL_USE_PLL | SYSCTL_XTAL_16MHZ | SYSCTL_OSC_MAIN);
 
    //
    // Set the PWM clock to the system clock.
    //
    SysCtlPWMClockSet(SYSCTL_PWMDIV_1);
 
    
    //
    // The PWM peripheral must be enabled for use.
    //
    SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM0);
 
    //
    // For this example PWM0 is used with PortB Pins 6 and 7.  The actual port
    // and pins used may be different on your part, consult the data sheet for
    // more information.  GPIO port B needs to be enabled so these pins can be
    // used.
    // TODO: change this to whichever GPIO port you are using.
    //
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOH);
 
    //
    // Configure the GPIO pin muxing to select PWM functions for these pins.
    // This step selects which alternate function is available for these pins.
    // This is necessary if your part supports GPIO pin function muxing.
    // Consult the data sheet to see which functions are allocated per pin.
    // TODO: change this to select the port/pin you are using.
    //
    GPIOPinConfigure(GPIO_PH0_M0PWM0);
  
    //
    // Configure the GPIO pad for PWM function on pins PB6 and PB7.  Consult
    // the data sheet to see which functions are allocated per pin.
    // TODO: change this to select the port/pin you are using.
    //
    GPIOPinTypePWM(GPIO_PORTH_BASE, GPIO_PIN_0);
 
 
    //
    // Configure the PWM0 to count up/down without synchronization.
    // Note: Enabling the dead-band generator automatically couples the 2
    // outputs from the PWM block so we don't use the PWM synchronization.
    //
   PWMGenConfigure(PWM0_BASE, PWM_GEN_0, PWM_GEN_MODE_UP_DOWN |
                    PWM_GEN_MODE_NO_SYNC);
 
   
 
    //
    // Set the PWM period to 250Hz.  To calculate the appropriate parameter
    // use the following equation: N = (1 / f) * SysClk.  Where N is the
    // function parameter, f is the desired frequency, and SysClk is the
    // system clock frequency.
    // In this case you get: (1 / 250Hz) * 16MHz = 64000 cycles.  Note that
    // the maximum period you can set is 2^16 - 1.
    // TODO: modify this calculation to use the clock frequency that you are
    // using.
    //
    PWMGenPeriodSet(PWM0_BASE, PWM_GEN_0, 504);
 
    //
    // Set PWM0 PD0 to a duty cycle of 25%.  You set the duty cycle as a
    // function of the period.  Since the period was set above, you can use the
    // PWMGenPeriodGet() function.  For this example the PWM will be high for
    // 25% of the time or 16000 clock cycles (64000 / 4).
    //
   
    
   PWMPulseWidthSet(PWM0_BASE, PWM_OUT_0,
   250);
 
    //
    // Enable the dead-band generation on the PWM0 output signal.  PWM bit 0
    // (PD0), will have a duty cycle of 25% (set above) and PWM bit 1 will have
    // a duty cycle of 75%.  These signals will have a 10us gap between the
    // rising and falling edges.  This means that before PWM bit 1 goes high,
    // PWM bit 0 has been low for at LEAST 160 cycles (or 10us) and the same
    // before PWM bit 0 goes high.  The dead-band generator lets you specify
    // the width of the "dead-band" delay, in PWM clock cycles, before the PWM
    // signal goes high and after the PWM signal falls.  For this example we
    // will use 160 cycles (or 10us) on both the rising and falling edges of
    // PD0.  Reference the datasheet for more information on dead-band
    // generation.
    //
   PWMDeadBandEnable(PWM0_BASE, PWM_GEN_0, 160, 160);
 
   
 
   PWMOutputState(PWM0_BASE, PWM_OUT_0_BIT, true);
 
    //
    // Enables the counter for a PWM generator block.
    //
    PWMGenEnable(PWM0_BASE, PWM_GEN_0);
 
    //
    // Loop forever while the PWM signals are generated.
    //
    while(1)
    {
        
    }
}