Hi,
I am trying to use TI LwIP demo for FreeRTOS and I am seeing a broken receive path through the stack.
Issue only occurs under periods of load where we are seeing many broadcasts or trying to do some TCP.
Pbuf_alloc in receive path of the interrupt fails (hdkif_rx_handler) and at some point leads to the rxch->active_head being set to NULL. And due to the fact the processing loop checking the receive buffers does not check for a curr_bd of NULL this leads to treating the memery at 0 as a pBuf and the effect where er hang in the loop in the ISR.
I have added a check to the processing loop for a curr_bd for NULL and to break and exit the ISR.
But my question is "Where in LwIP will we make those Pbuff_allocs to replenish the receive ISRs buffers if it is not done from the ISR?
This is a normal processing case; we have no ore resources for the receive DMA; we drop packets. At some point in the future buffers are freed up and allocated for the receive DMA.......but where?
Somebody must have seen such issues?
Have any of you got a fix?
Kind Regards,
Owain