Other Parts Discussed in Thread: TM4C1294NCPDT, TM4C1294KCPDT
Dear all
I used the EK-TM4C1294 evaluation board. This board has uP TM4C1294NCPDT. With this board I can access the Ethernet with my own SW.
Then I developed my own board TM4C1294KCPDT. The schematic is more or less the same like in the EK-TM4C1294. But my board I used a different Ethernet Connector with included magnetic.
Result:
With TM4C1294NCPDT of EK-TM4C1294 evaluation boardI can access Ethernet.
With TM4C1294KCPDT and my board I have no access to Ethernet.
For to be sure not the Ethernet connector of my own board is the problem, I removed U10 from EK-TM4C1294 and I soldered Ethernet connector of my solution into the EK-TM4C1294 board. Also EK-TM4C1294 + my Ethernet connector is working fine.
I also changed target HW in the CCS properties. But with EK-TM4C1294 my SW is running with target TM4C1294NCPDT and TM4C1294KCPDT. So I think there is no relevant difference between these 2 processors in my case. (My program uses 130kB and very few RAM)
Question: Is there any difference between these 2 processors?
Attached the schematic of my solution.
Thank for any input.
BR Franz