Other Parts Discussed in Thread: RM48L950
Hello,
I am using the RM48L950 to communicate with a DAC eval board through SPI2.
The message I am trying to transmit is a 32 bit stream broken into two 16 bit blocks which should be transmitted one after the other while the chip select is held low until all 32 bits are sent.
I am getting sudden jumps on the SDI and CS lines that last for about 5ns. Could someone help me understand what is causing the issue?
Here is my code and a picture of the scope where you can see the jumps (red = SDO, blue = CLK, purple = SDI, yellow = CS).
Thanks,
Rafael
spiDAT1_t dataconfig1_t;
uint16 datain[2] = {0x0000, 0x0000};
/* USER CODE END */
void UNI_SPI_setup(void)
{
/* USER CODE BEGIN (3) */
dataconfig1_t.CS_HOLD = TRUE;
dataconfig1_t.WDEL = TRUE;
dataconfig1_t.DFSEL = SPI_FMT_0;
dataconfig1_t.CSNR = 0xFE;
/* Enable IRQ */
_enable_IRQ();
/* Initialize SCI module */
spiInit();
/* USER CODE END */
}
/* USER CODE BEGIN (4) */
void UNI_SPI_transmit(uint16 data[2])
{
spiSendAndGetData(spiREG2, &dataconfig1_t, 2, data, datain);
}