This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4c123gxl UART1 FIFO Interrupt missing

Hello

I have a UART communication with a motorcontroller. Befor the FIFO i sent it with the same function but to receive i waited in a for-loop until there is a character available. This methode blocked the hole MC for a long time. 

I want to give an interrupt by 3 bytes available which means the Rx FIFO is 1/8 full. I dont need the Tx-FIFO. 

My problem now: I never get an Interrupt. If i enable the Tx-Interrupt i get one and it runs the UART1IntHandler. So its not a problem with the Implementation of the Handler itselfe. Even Send worked fine befor enable FIFO. Do I miss something in the Initialisation for the FIFO? Is it how i send? Do i need to send it with the Tx FIFO aswell?

Thank you very much

Best regards

//This are my variables i need for my Ringbuffer

typedef struct { uint8_t buffer[64]; uint8_t count_in; uint8_t count_out; uint8_t charavail; }UART_Buffer; UART_Buffer UART1_Buffer; // This is the initialisation of the UART1 with FIFO void uartInit(void) { SysCtlPeripheralEnable(SYSCTL_PERIPH_UART1); GPIOPinConfigure(GPIO_PB0_U1RX); GPIOPinConfigure(GPIO_PB1_U1TX); GPIOPinTypeUART(GPIO_PORTB_BASE, GPIO_PIN_0 | GPIO_PIN_1); UARTConfigSetExpClk(UART1_BASE, SysCtlClockGet(), 115200, UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE); UARTFIFOLevelSet(UART1_BASE, UART_FIFO_TX7_8, UART_FIFO_RX1_8); IntEnable(INT_UART1); UARTEnable(UART1_BASE); UARTIntEnable(UART1_BASE, UART_INT_RX); UARTFIFOEnable(UART1_BASE); IntMasterEnable(); } // This is the Function builds the String to ask for some values from slave void uartReadRegister(uint32_t uartBase, uint16_t registerAddress) { uint16_t crc; uint8_t sendByte[8]; //uint8_t receiveByte[7]; sendByte[0] = 1; // Slave ID sendByte[1] = 0x03; // Function Code sendByte[2] = (registerAddress >> 8) & LOW_BYTE_MASK; // Start Address High Byte sendByte[3] = registerAddress & LOW_BYTE_MASK; // Start Address Low Byte sendByte[4] = 0; // Number of Registers High Byte sendByte[5] = 4; // Number of Registers Low Byte crc = getCRC(sendByte, 6); // Function to calculate CRC sendByte[6] = crc & LOW_BYTE_MASK; // CRC Low Byte sendByte[7] = (crc >> 8) & LOW_BYTE_MASK; // CRC High Byte uartSendFrame(uartBase, sendByte, 8); //uartReceiveFrame(uartBase, receiveByte, 7); //Method without FIFO // return ((receiveByte[3] << 8) + receiveByte[4]); // return value without FIFO }


// This is the function to send String(worked fine before FIFO enabled
void uartSendFrame(uint32_t uartBase, uint8_t* sendByte, uint8_t length) {
     uint8_t i;
     for (i = 0; i < length; i++) {
          UARTCharPut(uartBase, sendByte[i]);
     }
}

// UART Interrupt handler void UART1IntHandler(void) { uint32_t ui32Status; ui32Status = UARTIntStatus(UART1_BASE, true); //get interrupt status UARTIntClear(UART1_BASE, ui32Status); //clear the asserted interrupts while(UARTCharsAvail(UART1_BASE)){ UART1_Buffer.buffer[UART1_Buffer.count_in] = UARTCharGetNonBlocking(UART1_BASE); UART1_Buffer.count_in = ++UART1_Buffer.count_in & 0x3f; UART1_Buffer.charavail++; } } // This function is to analyze the string i received

void MotorControllerBufferRead(struct Motors* Motor, uint32_t uartBase, UART_Buffer Buffer){ if(Buffer.charavail >=8){ if(Buffer.buffer[Buffer.count_out+1] == 0x10){ Buffer.count_out = (Buffer.count_out + 8) & 0x3F; Buffer.charavail -= 8; } } else if(Buffer.charavail >= 13){ if(Buffer.buffer[(Buffer.count_out+1) & 0x3F] == 0x03){ Motor->speed = ((Buffer.buffer[(Buffer.count_out + 3) & 0x3F] << 8) + Buffer.buffer[(Buffer.count_out + 4) & 0x3F] ) / 60.0f; Motor->dcVoltage = ((Buffer.buffer[(Buffer.count_out + 7) & 0x3F] << 8) + Buffer.buffer[(Buffer.count_out + 8) & 0x3F] ) / 32.0f; Motor->dcCurrent = ((Buffer.buffer[(Buffer.count_out + 9) & 0x3F] << 8) + Buffer.buffer[(Buffer.count_out + 10) & 0x3F] ) / 32.0f; Buffer.count_out = (Buffer.count_out + 13) & 0x3F; Buffer.charavail -= 13; } } }

// This is the old function to receive a byte.

void uartReceiveFrame(uint32_t uartBase, uint8_t* receiveByte, uint8_t length) {
     int32_t tempByte = 0;
     uint16_t attempt = 0;
     uint8_t i = 0;

     do {
          tempByte = UARTCharGetNonBlocking(uartBase);
          if (tempByte != -1) {
               attempt = 0;
               receiveByte[i] = tempByte;
               ++i;
          } else {
               ++attempt;
               if (attempt > 5000) {
                    break;
               }
          }
     } while (i < length);
}