Part Number: RM48L952
Other Parts Discussed in Thread: DRV8301, TMS570LS3137, HALCOGEN,
Tool/software: Code Composer Studio
Hey there'
I am using TMDXRM48 as control card which is placed on DRV8301 to drive the BLDC motor
this is my code composer studio screen shot
I have used HET1_04 with the help of GPIO pins to provide a pwm at my DRV8301 pinouts which is PWM_BH
This is the screen shot of tms(control card) of HET1_04(highlighted)
and this is the screen shot of DRV8301 AS SHOWN BELOW
but in CCS there is a het.c file which has some dedicated pins of HET as shown in the screen shot below
You can see in the screen shot that HET pin 14 is used for pwm 3 but when I am changing the the pin from 14 to pin 4 while using the same pwm 3 channel and saving the code,the desired output is not being appeared.
So please provide help,Do I have to change the address also?