Part Number: TMS570LC4357
Other Parts Discussed in Thread: LAUNCHXL2-570LC43
Dear All,
one of my customer working on LaunchXL2-570LC43 kit for their electric vehicle service equipment which is basically a controller card for communication btw EV charger and server.. They primarly need MCU device with CAN, Ethernet and LCD drive capability.
They would need to connect 7inch LCD display to Launchpad kit, please help to advise any reliable/low cost source for LCD vendor/LCD booster packs avalable with which we can interface and test, we need LCD module with in-built driver which can be interfaced with hercules MCU via SPI/I2C/Paralle bus to drive same. Aside this Can Hercules MCU will be able to drive RGB o/p based LCD directly without any external drivers?
Also please advise whether any SD card booster backs available which we can interface with above Hercules launchpad kit.
Also we are hearing that Hercules MCU is best fit for Electric vehicle applications compared to Tiva MCU, please advise why is it so and what will be main benefits of going with Hercules MCU?
Rgds,
Aravind.