Part Number: TM4C129DNCPDT
Hi
I am using tm4c129dncpdt for my project and in this project I am using lwip stack and I am going to interface external phy for ethernet and the phy is ksz8081rnbca .
My interface for the device and phy will be RMII. I have configured like below
ROM_GPIOPinConfigure(GPIO_PG3_EN0TXEN);
ROM_GPIOPinConfigure(GPIO_PG5_EN0TXD1);
ROM_GPIOPinConfigure(GPIO_PG4_EN0TXD0);
ROM_GPIOPinConfigure(GPIO_PG7_EN0RXDV);
ROM_GPIOPinConfigure(GPIO_PQ5_EN0RXD0);
ROM_GPIOPinConfigure(GPIO_PQ6_EN0RXD1);
ROM_GPIOPinConfigure(GPIO_PK4_EN0INTRN);
ROM_GPIOPinConfigure(GPIO_PF2_EN0MDC);
ROM_GPIOPinConfigure(GPIO_PF3_EN0MDIO);
ROM_GPIOPinConfigure(GPIO_PM4_EN0RREF_CLK);
ROM_GPIOPinConfigure(GPIO_PF1_EN0LED2);
ROM_GPIOPinConfigure(GPIO_PK4_EN0LED0);
ROM_GPIOPinConfigure(GPIO_PK6_EN0LED1);
GPIOPinTypeEthernetLED(GPIO_PORTF_BASE, GPIO_PIN_1);
GPIOPinTypeEthernetLED(GPIO_PORTK_BASE, GPIO_PIN_4);
GPIOPinTypeEthernetLED(GPIO_PORTK_BASE, GPIO_PIN_6);
and after this I have defined the macro EMAC_PHY_TYPE_EXTERNAL_RMII..
The code is getting looped in EMACPHYConfigSet function.
Can anyone help me with this interface..
Regards
Harish