Other Parts Discussed in Thread: TM4C123GH6PM
Tool/software: Code Composer Studio
Hello,
I have started to write stand alone ASM programs but I am getting two errors: I am using the Tiva C launchpad.
CORTEX_M4_0: File Loader: Verification failed: Values at address 0x00000100 do not match Please verify target memory and memory map.
CORTEX_M4_0: GEL: File: C:\Users\Michael\workspace_v7\ASMBlink\Debug\ASMBlink.out: a data verification error occurred, file load failed.
CORTEX_M4_0: Error: Debug Port error occurred.
I don't understand either.
The first error started when I opened up another project and then switched back to this one. The second error always existed and everything appears to work but it needs to be fixed.
With a standard C project everything is fine.
code:
/******************************************************************************
*
* Default Linker Command file for the Texas Instruments TM4C123GH6PM
*
* This is derived from revision 15071 of the TivaWare Library.
*
*****************************************************************************/
MEMORY
{
FLASH (RX) : origin = 0x00000000, length = 0x00040000
SRAM (RWX) : origin = 0x20000000, length = 0x00008000
}
/* The following command line options are set as part of the CCS project. */
/* If you are building using the command line, or for some reason want to */
/* define them here, you can uncomment and modify these lines as needed. */
/* If you are using CCS for building, it is probably better to make any such */
/* modifications in your CCS project and leave this file alone. */
/* */
/* --heap_size=0 */
/* --stack_size=256 */
/* --library=rtsv7M4_T_le_eabi.lib */
/* Section allocation in memory */
SECTIONS
{
.intVec: > 0x00000000
.text : > 0x100
}
config file:
<?xml version="1.0" encoding="UTF-8" standalone="no"?>
<configurations XML_version="1.2" id="configurations_0">
<configuration XML_version="1.2" id="Stellaris In-Circuit Debug Interface_0">
<instance XML_version="1.2" desc="Stellaris In-Circuit Debug Interface_0" href="connections/Stellaris_ICDI_Connection.xml" id="Stellaris In-Circuit Debug Interface_0" xml="Stellaris_ICDI_Connection.xml" xmlpath="connections"/>
<connection XML_version="1.2" id="Stellaris In-Circuit Debug Interface_0">
<instance XML_version="1.2" href="drivers/stellaris_cs_dap.xml" id="drivers" xml="stellaris_cs_dap.xml" xmlpath="drivers"/>
<instance XML_version="1.2" href="drivers/stellaris_cortex_m4.xml" id="drivers" xml="stellaris_cortex_m4.xml" xmlpath="drivers"/>
<platform XML_version="1.2" id="platform_0">
<instance XML_version="1.2" desc="Tiva TM4C123GH6PM_0" href="devices/tm4c123gh6pm.xml" id="Tiva TM4C123GH6PM_0" xml="tm4c123gh6pm.xml" xmlpath="devices"/>
</platform>
</connection>
</configuration>
</configurations>