Hello,
I find the following statement in the TRM for TMS570 within the section [18.4.2.3 Parity Checking]:
"The parity check is performed when the NHET execution unit makes a read access to NHET RAM, but also when a different master (e.g. CPU, HTU, DMA,...) performs the read access." I am trying to check Parity Error feature while CPU is READing NHET RAM with Parity Error. It doesn't occur. But when NHET READ the same NHET RAM location, Parity Error does occur. Can anyone tell me, if that is the expected behaviour as it doesn't match the line from the TRM as shown above? Thank you. Regards Pashan