Part Number: RM57L843
Other Parts Discussed in Thread: TMS570LC4357,
Hi, I have some questions about Errata DCC#24.
- According to the description of errata DCC#24 trigger condition, it can only be triggered when using single shot mode and counter 1 source is not VLCK. As the VCLK is derived from PLL output, if I choose the PLL output as the counter 1 source, will this errata be triggered?
- The workaround for SSWF021#45 uses DCC to detect the PLL output frequency. Does it need to apply the workaround for DCC#24?
- When trimming LPO using DCC, do I need to apply the workaround for DCC#24?
- How to specifically remove the static frequency offset and sporadic offset?
- Are those removing-offset action applied only when I need reading out the counter 1 value, like detecting frequency-unknown source?
- If I just want to use DCC detection result (Error or No Error), like what's done in the workaround for SSWF021#45, how do I remove the static frequency offset and sporadic offset?