Part Number: EK-TM4C123GXL
Tool/software: Code Composer Studio
Hello,I am facing a problem with my code. I am trying to get the gyro informations from sensor hub and control one servo via uart1 .
Separately,the codes are working fine,but when i try to combine the,i am facing a problem when i try to configure the pin for pwm(ROM_GPIOPinConfigure(GPIO_PB4_M0PWM2);) i see that the buffer is stuck.
Here is the code,if you (ctrl+F) on "mere" ,there is where the problem starts. and i also saved the procject here :
#include <stdint.h>
#include <stdbool.h>
#include <math.h>
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc/hw_ints.h"
#include "driverlib/debug.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/sysctl.h"
#include "driverlib/systick.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.h"
#include "sensorlib/hw_bmp180.h"
#include "sensorlib/i2cm_drv.h"
#include "sensorlib/bmp180.h"
#include "drivers/rgb.h"
#include "sensorlib/ak8975.h"
#include "sensorlib/mpu9150.h"
#include "sensorlib/mpu6050.h"
#include "sensorlib/hw_mpu9150.h"
#include <stdint.h>
#include <stdbool.h>
#include <math.h>
#include <time.h>
#include <string.h>
#include <stdlib.h>
#include "inc/hw_types.h"
#include "inc/hw_memmap.h"
#include "inc/hw_hibernate.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/hibernate.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/sysctl.h"
#include "driverlib/systick.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.h"
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/sysctl.h"
#include "driverlib/gpio.h"
#include "driverlib/debug.h"
#include "driverlib/pwm.h"
#include "driverlib/pin_map.h"
#include "inc/hw_gpio.h"
#include "driverlib/rom.h"
#define PWM_FREQUENCY 55
//*****************************************************************************
//
//! \addtogroup example_list
//! <h1>Pressure Measurement with the BMP180 (pressure_bmp180)</h1>
//!
//! This example demonstrates the basic use of the Sensor Library, TM4C123G
//! LaunchPad and the SensHub BoosterPack to obtain air pressure and
//! temperature measurements with the BMP180 sensor.
//!
//! Connect a serial terminal program to the LaunchPad's ICDI virtual serial
//! port at 115,200 baud. Use eight bits per byte, no parity and one stop bit.
//! The raw sensor measurements are printed to the terminal. The RGB LED
//! blinks at 1Hz once the initialization is complete and the example is
//! running.
//
//*****************************************************************************
//*****************************************************************************
//
// Define BMP180 I2C Address.
//
//*****************************************************************************
#define BMP180_I2C_ADDRESS 0x77
//*****************************************************************************
#define MPU9150_I2C_ADDRESS 0X68
//*****************************************************************************
//
// Global array for holding the color values for the RGB.
//
//*****************************************************************************
uint32_t g_pui32Colors[3];
//*****************************************************************************
//
// Global instance structure for the I2C master driver.
//
//*****************************************************************************
tI2CMInstance g_sI2CInst;
//*****************************************************************************
//
// Global instance structure for the BMP180 sensor driver.
//
//*****************************************************************************
tBMP180 g_sBMP180Inst;
//*****************************************************************************
// Global instance structure for MPU9150 sensor driver
//
//*****************************************************************************
tMPU9150 sMPU9150;
//*****************************************************************************
//
// Global new data flag to alert main that BMP180 data is ready.
//
//*****************************************************************************
volatile uint_fast8_t g_vui8DataFlag;
//*****************************************************************************
//
// A boolean that is set when a MPU9150 command has completed.
//
//*****************************************************************************
volatile bool g_bMPU9150Done;
//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif
int32_t functie(int32_t n)
{
int32_t rez;
rez = 2*n;
return(rez);
}
void comenzi(char *str, float *com1, float *com2)
{
float temp[3];
char buffer[16];
char com[5];
int32_t i, j, k, p;
int32_t n, ns, nf;
i=0;j=0;k=0;p=0;
n=0;ns=0;nf=0;
strcpy(buffer, str);
n=strlen(buffer);
for(i=0;i<n; i++)
{
if(buffer[i] ==',')
{
nf = i;
for(j=ns;j<nf;j++)
{
com[p] = buffer[j];
p++;
}
com[p]='\0';
temp[k] = atof(com);
p = 0;
com[p] ='\0';
k++;
ns = i+1;
}
}
*com1 =temp[0];
*com2 =temp[1]/2;
}
//*****************************************************************************
//
// BMP180 Sensor callback function. Called at the end of BMP180 sensor driver
// transactions. This is called from I2C interrupt context. Therefore, we just
// set a flag and let main do the bulk of the computations and display.
//
//*****************************************************************************
void BMP180AppCallback(void* pvCallbackData, uint_fast8_t ui8Status)
{
if(ui8Status == I2CM_STATUS_SUCCESS)
{
g_vui8DataFlag = 1;
}
}
//*******************************************************************************
//
// The function that is provided by this example as a callback when MPU9150
// transactions have completed.
void MPU9150Callback(void *pvCallbackData, uint_fast8_t ui8Status)
{
//
// See if an error occurred.
//
if(ui8Status != I2CM_STATUS_SUCCESS)
{
//
// An error occurred, so handle it here if required.
//
}
//
// Indicate that the MPU9150 transaction has completed.
//
g_bMPU9150Done = true;
}
//*****************************************************************************
//
// Called by the NVIC as a result of I2C3 Interrupt. I2C3 is the I2C connection
// to the BMP180.
//
//*****************************************************************************
void
BMP180I2CIntHandler(void)
{
//
// Pass through to the I2CM interrupt handler provided by sensor library.
// This is required to be at application level so that I2CMIntHandler can
// receive the instance structure pointer as an argument.
//
I2CMIntHandler(&g_sI2CInst);
}
//*****************************************************************************
//
// Called by the NVIC as a result of I2C3 Interrupt. I2C3 is the I2C connection
// to the MPU9150.
//
//*****************************************************************************
void
MPU9150I2CIntHandler(void)
{
//
// Pass through to the I2CM interrupt handler provided by sensor library.
// This is required to be at application level so that I2CMIntHandler can
// receive the instance structure pointer as an argument.
//
I2CMIntHandler(&g_sI2CInst);
}
//*****************************************************************************
//
// Called by the NVIC as a SysTick interrupt, which is used to generate the
// sample interval
//
//*****************************************************************************
void
SysTickIntHandler()
{
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, GPIO_PIN_1);
BMP180DataRead(&g_sBMP180Inst, BMP180AppCallback, &g_sBMP180Inst);
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, 0x00);
}
//*****************************************************************************
//
// Configure the UART and its pins. This must be called before UARTprintf().
//
//*****************************************************************************
void
ConfigureUART(void)
{
//
// Enable the GPIO Peripheral used by the UART.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
//
// Enable UART0
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
//
// Configure GPIO Pins for UART mode.
//
ROM_GPIOPinConfigure(GPIO_PA0_U0RX);
ROM_GPIOPinConfigure(GPIO_PA1_U0TX);
ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
//
// Use the internal 16MHz oscillator as the UART clock source.
//
UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);
//
// Initialize the UART for console I/O.
//
UARTStdioConfig(0, 9600, 16000000);
}
//*****************************************************************************
//
// Main 'C' Language entry point.
//
//*****************************************************************************
int
main(void)
{
volatile uint32_t ui32Load;
volatile uint32_t ui32PWMClock;
volatile uint8_t ui8Adjust;
ui8Adjust = 83;
///////////////////////---------
float fTemperature, fPressure, fAltitude;
int32_t i32IntegerPart, i32IntegerPartAx, i32IntegerPartAy, i32IntegerPartAz;
int32_t i32FractionPart, i32FractionPartAx,i32FractionPartAy, i32FractionPartAz;
uint_fast16_t TemperatureRaw;
float fAccel[3], fGyro[3];
uint_fast16_t fMagneto[3];
//
// Setup the system clock to run at 40 MHz from PLL with crystal reference
//
ROM_SysCtlClockSet(SYSCTL_SYSDIV_5 | SYSCTL_USE_PLL | SYSCTL_XTAL_16MHZ |
SYSCTL_OSC_MAIN);
//
// Initialize the UART.
//
ConfigureUART();
//
// Print the welcome message to the terminal.
//
UARTprintf("\033[2JBMP180 Example\n");
//
// Set the color to a white approximation.
//
g_pui32Colors[RED] = 0x8000;
g_pui32Colors[BLUE] = 0x8000;
g_pui32Colors[GREEN] = 0x8000;
//
// Initialize RGB driver. Use a default intensity and blink rate.
//
RGBInit(0);
RGBColorSet(g_pui32Colors);
RGBIntensitySet(0.5f);
RGBEnable();
//
// The I2C3 peripheral must be enabled before use.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C3);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
//
// Configure the pin muxing for I2C3 functions on port D0 and D1.
// This step is not necessary if your part does not support pin muxing.
//
ROM_GPIOPinConfigure(GPIO_PD0_I2C3SCL);
ROM_GPIOPinConfigure(GPIO_PD1_I2C3SDA);
//
// Select the I2C function for these pins. This function will also
// configure the GPIO pins pins for I2C operation, setting them to
// open-drain operation with weak pull-ups. Consult the data sheet
// to see which functions are allocated per pin.
//
GPIOPinTypeI2CSCL(GPIO_PORTD_BASE, GPIO_PIN_0);
ROM_GPIOPinTypeI2C(GPIO_PORTD_BASE, GPIO_PIN_1);
//
// Initialize the GPIO for the LED.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
ROM_GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_1);
ROM_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, 0x00);
ROM_SysCtlPWMClockSet(SYSCTL_PWMDIV_64);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM1);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
ROM_GPIOPinTypePWM(GPIO_PORTD_BASE, GPIO_PIN_0);
//
// Enable interrupts to the processor.
//
ROM_IntMasterEnable();
//
// Initialize the I2C3 peripheral.
//
I2CMInit(&g_sI2CInst, I2C3_BASE, INT_I2C3, 0xff, 0xff,
ROM_SysCtlClockGet());
//
// Initialize the BMP180.
//
BMP180Init(&g_sBMP180Inst, &g_sI2CInst, BMP180_I2C_ADDRESS,
BMP180AppCallback, &g_sBMP180Inst);
//
// Wait for initialization callback to indicate reset request is complete.
//
while(g_vui8DataFlag == 0)
{
//
// Wait for I2C Transactions to complete.
//
}
//
// Reset the data ready flag
//
g_vui8DataFlag = 0;
//Initialize the MPU9150.
g_bMPU9150Done == false;
MPU9150Init(&sMPU9150, &g_sI2CInst, MPU9150_I2C_ADDRESS, MPU9150Callback, 0);
while(!g_bMPU9150Done)
{
}
g_bMPU9150Done = false;
MPU9150ReadModifyWrite(&sMPU9150, MPU9150_O_ACCEL_CONFIG,
~MPU9150_ACCEL_CONFIG_AFS_SEL_M,
MPU9150_ACCEL_CONFIG_AFS_SEL_4G, MPU9150Callback,
0);
//
// Enable the system ticks at 10 Hz.
//
ROM_SysTickPeriodSet(ROM_SysCtlClockGet() / (10 * 3));
ROM_SysTickIntEnable();
ROM_SysTickEnable();
//
// After all the init and config we start blink the LED
//
RGBBlinkRateSet(1.0f);
//
// Begin the data collection and printing. Loop Forever.
// mere
ROM_GPIOPinConfigure(GPIO_PB4_M0PWM2);
ui32PWMClock = SysCtlClockGet() / 64;
ui32Load = (ui32PWMClock / PWM_FREQUENCY) - 1;
PWMGenConfigure(PWM0_BASE, PWM_GEN_0, PWM_GEN_MODE_DOWN);
PWMGenPeriodSet(PWM0_BASE, PWM_GEN_0, ui32Load);
ROM_PWMPulseWidthSet(PWM0_BASE, PWM_OUT_0, ui8Adjust * ui32Load / 1000);
ROM_PWMOutputState(PWM0_BASE, PWM_OUT_0_BIT, true);
ROM_PWMGenEnable(PWM0_BASE, PWM_GEN_0);
char g_cInput[16];
float d1, d2;
ROM_FPUEnable();
ROM_FPUStackingEnable();
UARTprintf("TEST");
while(1)
{
if(UARTPeek('\r') !=-1)
{
///
///
UARTgets(g_cInput,sizeof(g_cInput));
UARTprintf("Ce s-a printat: %s\n",g_cInput);
comenzi(g_cInput, &d1, &d2);
UARTprintf("%d, %d\n", (int32_t)d1, (int32_t)d2);
}
ui8Adjust = (int32_t)d1;
ROM_PWMPulseWidthSet(PWM1_BASE, PWM_OUT_0, ui8Adjust * ui32Load / 1000);
ROM_SysCtlDelay(100000);
//
// Read the data from the BMP180 over I2C. This command starts a
// temperature measurement. Then polls until temperature is ready.
// Then automatically starts a pressure measurement and polls for that
// to complete. When both measurement are complete and in the local
// buffer then the application callback is called from the I2C
// interrupt context. Polling is done on I2C interrupts allowing
// processor to continue doing other tasks as needed.
//
BMP180DataRead(&g_sBMP180Inst, BMP180AppCallback, &g_sBMP180Inst);
while(g_vui8DataFlag == 0)
{
//
// Wait for the new data set to be available.
//
}
//
// Reset the data ready flag.
//
g_vui8DataFlag = 0;
while(!g_bMPU9150Done)
{
}
g_bMPU9150Done = false;
MPU9150DataRead(&sMPU9150, MPU9150Callback, 0);
while(!g_bMPU9150Done)
{
}
MPU9150DataAccelGetFloat(&sMPU9150, &fAccel[0], &fAccel[1], &fAccel[2]);
//
// Get a local copy of the latest temperature data in float format.
//
BMP180DataTemperatureGetFloat(&g_sBMP180Inst, &fTemperature);
BMP180DataTemperatureGetRaw(&g_sBMP180Inst, &TemperatureRaw);
//
// Convert the floats to an integer part and fraction part for easy
// print.
//
/*
i32IntegerPart = (int32_t) fTemperature;
i32FractionPart =(int32_t) (fTemperature * 1000.0f);
i32FractionPart = i32FractionPart - (i32IntegerPart * 1000);
if(i32FractionPart < 0)
{
i32FractionPart *= -1;
}
*/
i32IntegerPartAx = (int32_t) fAccel[0];
i32FractionPartAx =(int32_t) (fAccel[0] * 1000.0f);
i32FractionPartAx = i32FractionPartAx - (i32IntegerPartAx * 1000);
if(i32FractionPartAx < 0)
{
i32FractionPartAx *= -1;
}
i32IntegerPartAy = (int32_t) fAccel[1];
i32FractionPartAy =(int32_t) (fAccel[1] * 1000.0f);
i32FractionPartAy = i32FractionPartAy - (i32IntegerPartAy * 1000);
if(i32FractionPartAy < 0)
{
i32FractionPartAy *= -1;
}
i32IntegerPartAz = (int32_t) fAccel[2];
i32FractionPartAz =(int32_t) (fAccel[2] * 1000.0f);
i32FractionPartAz = i32FractionPartAz - (i32IntegerPartAz * 1000);
if(i32FractionPartAz < 0)
{
i32FractionPartAz *= -1;
}
//banana
// Print temperature with three digits of decimal precision.
//
// UARTprintf("Temperature %3d.%03d\t\t", i32IntegerPart, i32FractionPart);
// UARTprintf("%3d.%3d %3d.%3d %3d.%3d", i32IntegerPartAx, i32FractionPartAx, i32IntegerPartAy, i32FractionPartAy, i32IntegerPartAz, i32FractionPartAz);
UARTprintf("%3d.%03d", i32IntegerPartAx, i32FractionPartAx);
UARTprintf(",");
UARTprintf("%3d.%03d", i32IntegerPartAy, i32FractionPartAy);
UARTprintf(",");
UARTprintf("%3d.%03d", i32IntegerPartAz, i32FractionPartAz);
//UARTprintf("\033[5;63H%3d.%03d", i32IntegerPartAx, i32FractionPartAx);
//UARTprintf("\033[5;63H%3d.%03d", i32IntegerPartAy, i32FractionPartAy);
//UARTprintf("%3d.%3d \n", i32IntegerPartAy, i32FractionPartAy);
//UARTprintf("%3d.%3d \n", i32IntegerPartAz, i32FractionPartAz);
// UARTprintf("x %3d.%03d\t\t", i32IntegerPart, i32FractionPart);
// UARTprintf("%d",fAccel[2]);
// UARTprintf("Pressure %.6f",fTemperature);
//
// Get a local copy of the latest air pressure data in float format.
//
//BMP180DataPressureGetFloat(&g_sBMP180Inst, &fPressure);
MPU9150DataMagnetoGetRaw(&sMPU9150, &fMagneto[0], &fMagneto[1], &fMagneto[2]);
//
// Convert the floats to an integer part and fraction part for easy
// print.
//
i32IntegerPart = (int32_t) fMagneto[0];
i32FractionPart =(int32_t) (fMagneto[0] * 1000.0f);
i32FractionPart = i32FractionPart - (i32IntegerPart * 1000);
if(i32FractionPart < 0)
{
i32FractionPart *= -1;
}
//
// Print Pressure with three digits of decimal precision.
//
//UARTprintf("MagX %3d.%03d\t\t", i32IntegerPart, i32FractionPart);
//
// Calculate the altitude.
//
fAltitude = 44330.0f * (1.0f - powf(fPressure / 101325.0f,
1.0f / 5.255f));
//
// Convert the floats to an integer part and fraction part for easy
// print.
//
i32IntegerPart = (int32_t) fAltitude;
i32FractionPart =(int32_t) (fAltitude * 1000.0f);
i32FractionPart = i32FractionPart - (i32IntegerPart * 1000);
if(i32FractionPart < 0)
{
i32FractionPart *= -1;
}
//
// Print altitude with three digits of decimal precision.
//
//UARTprintf("Altitude %3d.%03d", i32IntegerPart, i32FractionPart);
//
// Print new line.
//
UARTprintf("\n");
//
// Delay to keep printing speed reasonable. About 100 milliseconds.
//
ROM_SysCtlDelay(ROM_SysCtlClockGet() / (10 * 3));
}//while end
}
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/908/test.7z