Other Parts Discussed in Thread: HALCOGEN,
Tool/software: Code Composer Studio
Hi Guys,
I use the Freertos in the TMS570LS1224,The code generated by the HALCoGen 04.07.00 and there are some error in it.
1# If i do not select the Use Timers of the Dialog in the HALCoGen 04.07.00.the tasks can run normally.
2# but if i use the time management of Freertos,that is selecting the Use Timers. the tasks can not run normally.
When i debug the code that i found the code stay on the same palce. show as below:
I don‘t know why!who can help me?
And the attachment is my project and the *.hcg file.