Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: LMFLASHPROGRAMMER, MAX232
Please reply ASAP it is urgent.
Respected sir/madam,
I am designing custom board using tm4c1294ncpdt uC. I have confusion regarding boot loading(programming) circuit. I know that i can boot load the uC using serial boot loader program also i can configure GPIO to put boot loader into update mode. But what i want to know is that what happens when i am programming the uC for first time.
1. is the uC by default into update mode after manufacturing??
2. Can i use serial UART boot loader code directly for programming first time??
3. Or some extra arrangement is required like, for the first time program using JTAG and then u can use UART for programming.
4. So please give me details of programming custom board (tm4c1294ncpdt) for the first time.
5. And if boot loading (programming) circuitry is available please share.
regards,
digvijay