This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

What is the I/O Pin Structure for MibSPI pins when configured as GPIO Pins?



Hello,

When I configure the MibSPI Pins as GPIO using PC0 Register, what should be the values for PC6, PC7 and PC8 Register?

I know that the answer to this question depends on the external electrical circuit.

But I could not find any PICTURE or BLOCK DIAGRAM describing the internal structure of the MibSPI Pins when it is in GPIO Mode.

Can you please provide me with some BLOCK DIAGRAM for the I/O Pin Structure for MibSPI?

Any information will help me to understand better than what is provided in the TRM.

Thank you.

Regards

Pashan