Part Number: TMS570LS3137
Hi,
I am working with TMDS570LS31USB. Code Composer Studio 8.0
F021 Flash API version is 02.01.01.
I downloaded the Hercules_MCU_Bootloader.zip from http://processors.wiki.ti.com/index.php/TMS570_Hercules_MCU_Bootloader
I am running the UART bootloader located in SafetyMCU_Bootloader\TMS570LS31x\boot_uart inside this zip file.
The bootloader builds and runs. I want to test downloading a small sample application, around 235KB. I press "1", and choose the .out file and send it through YModem on Teraterm.
I verify that Ymodem transferred the whole content since number of bytes macthes the file size. All good so far.
The problem is at Fapi_BlockErase(), execution hangs in this function forever, at line: while(FAPI_GET_FSM_STATUS != Fapi_Status_Success);
I already implemented the suggested first and second fixes proposed in the following post:
However the execution is still stuck at while(FAPI_GET_FSM_STATUS != Fapi_Status_Success); line inside Fapi_BlockErase().
Basically, (1) I replaced Fapi_enableMainBankSectors(0xFFFE) with of 0xFFFF. (2) in bl_link.cmd, I added section bl_flash.obj (.const) into the flashAPI section.
what is missing?
Do we need add more sections into the flashAPI via bl_link.cmd file? what other sections?
thank you in advance,