Part Number: TMDXRM57LHDK
Other Parts Discussed in Thread: HALCOGEN
Tool/software: TI C/C++ Compiler
Hi,
I'm using the RM57L Hardware Developement Kit. I try DMA write to the SDRAM 16Bit interface I'm but when I use my code I see no tranfer of data also no traffic on the address lines only the WEn is toggling(using a Digitalanalyzer). Using this in main:
emif_SDRAMInit();
/* - creating a data chunk in system ram to start with ... */
loadDataPattern(D_SIZE, &TXDATA_RAM[0], 0xFFFFFFFF ); // 0x5A5A5A5A
/* - configuring dma control packets */
g_dmaCTRLPKT1.SADD = (uint32)TXDATA_RAM; /* source address */
g_dmaCTRLPKT1.DADD = (uint32)(0x80000000); //(0x08078000); /* destination address; SDRAM */
g_dmaCTRLPKT1.CHCTRL = 0; /* channel control */
g_dmaCTRLPKT1.FRCNT = F_COUNT; /* frame count */
g_dmaCTRLPKT1.ELCNT = E_COUNT; /* element count */
g_dmaCTRLPKT1.ELDOFFSET = 0; /* element destination offset */
g_dmaCTRLPKT1.ELSOFFSET = 0; /* element destination offset */
g_dmaCTRLPKT1.FRDOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT1.FRSOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT1.PORTASGN = PORTA_READ_PORTA_WRITE;
g_dmaCTRLPKT1.RDSIZE = ACCESS_32_BIT; /* read size */
g_dmaCTRLPKT1.WRSIZE = ACCESS_32_BIT; /* write size */
g_dmaCTRLPKT1.TTYPE = FRAME_TRANSFER ; /* transfer type */
g_dmaCTRLPKT1.ADDMODERD = ADDR_INC1; /* address mode read */
g_dmaCTRLPKT1.ADDMODEWR = ADDR_INC1; /* address mode write */
g_dmaCTRLPKT1.AUTOINIT = AUTOINIT_OFF; /* autoinit */
g_dmaCTRLPKT2.SADD = (uint32)(0x80001000); //(0x80001000)(0x08076000); /* source address */
g_dmaCTRLPKT2.DADD = (uint32)RXDATA_RAM; /* destination address */
g_dmaCTRLPKT2.CHCTRL = 0; /* channel control */
g_dmaCTRLPKT2.FRCNT = F_COUNT; /* frame count */
g_dmaCTRLPKT2.ELCNT = E_COUNT; /* element count */
g_dmaCTRLPKT2.ELDOFFSET = 0; /* element destination offset */
g_dmaCTRLPKT2.ELSOFFSET = 0; /* element destination offset */
g_dmaCTRLPKT2.FRDOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT2.FRSOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT2.PORTASGN = PORTA_READ_PORTA_WRITE;
g_dmaCTRLPKT2.RDSIZE = ACCESS_32_BIT; /* read size */
g_dmaCTRLPKT2.WRSIZE = ACCESS_32_BIT; /* write size */
g_dmaCTRLPKT2.TTYPE = FRAME_TRANSFER ; /* transfer type */
g_dmaCTRLPKT2.ADDMODERD = ADDR_INC1; /* address mode read */
g_dmaCTRLPKT2.ADDMODEWR = ADDR_INC1; /* address mode write */
g_dmaCTRLPKT2.AUTOINIT = AUTOINIT_OFF; /* autoinit */
/* - setting dma control packets */
dmaSetCtrlPacket(DMA_CH1,g_dmaCTRLPKT1); //tx
//dmaSetCtrlPacket(DMA_CH0,g_dmaCTRLPKT2); //rx
/* - setting the dma channel to trigger on h/w request */
dmaSetChEnable(DMA_CH1, DMA_SW);
//dmaSetChEnable(DMA_CH0, DMA_SW);
/* Enable Block Transfer Complete interrupt for the receive after transfer complete */
//dmaEnableInterrupt(DMA_CH0, BTC, DMA_INTA);
dmaEnable();
In the sys_link I use this address
VECTORS (X) : origin=0x00000000 length=0x00000020
FLASH0 (RX) : origin=0x00000020 length=0x001FFFE0
FLASH1 (RX) : origin=0x00200000 length=0x00200000
STACKS (RW) : origin=0x08000000 length=0x00001500
RAM (RW) : origin=0x08001500 length=0x0007BB00
SHAREDRAM (RW) : origin=0x0807D000 length=0x00003000
/* USER CODE BEGIN (3) */
SDRAM (RWX) : origin=0x80000000 length=0200000000
Thank you
Marcel