Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: UNIFLASH
How do I program a MAC address for a custom design using the TM4C1294?
I tried it with the following link, and the randomly entered MAC address worked well.
However, I set and read another MAC address, but the desired value was not written.
So I wrote 00: 00: 00: 00: 00: 00 to initialize it, but I can not write any value afterwards.
Finally, I tried to unlock (aka. Factory reset) but this also failed.
How do I resolve this problem?
Thanks in advance.