Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: UNIFLASH
Hello,
i want to change the MAC address for the etherent interface on a TM4C1294NCPDT.
Unfortunately it cannot be changed by initializing the Ethernet interface directly with another MAC address, which is not the MAC address in the UserRegister 0 and 1.
If you initialize the Ethernet interface with the values in User Register 0 and 1, the interface will work, otherwise it will not work.
But I can't change these values in the User Registers either, neither in source code nor with Uniflash.
Has TI assigned fixed MAC addresses to the microcontrollers that cannot be changed?
Can User Registers 0 and 1 be written to only once.
Why is user register 0 and 1 directly related to the Ethernet interface so that the interface only works with those values as MAC address and not otherwise?
With kind regards
Ali