Part Number: TMS570LS3137
Other Parts Discussed in Thread: HALCOGEN
Hello,
We are using below tool in our development:
CCS version : 8.0
Flash API : 02.01.01
HALCOGEN : 04.06
We have two images,
1. one which is generated using HALCOGEN tool and
2. another images which executes from RAM with Flash F021 libraries and API's calling to flash images.
Both the images work independently. when we flash HALCOGEN generated image (i.e. image mentioned in 1) using the image executing in RAM (i.e. image mentioned in 2), code is stuck at CheckFlashECC() which is generated by HALCOGEN. can you please help us in identifying the issue?
Thanks,
Kalyan