Part Number: DK-TM4C129X
Other Parts Discussed in Thread: TM4C1294KCPDT, TM4C129XKCZAD
I'm working with uDMA on the TM4C129 series processor on the DK-TM4C129x development kit. The code performs a software memory to memory scatter / gather transfer then does a little clean up in an interrupt routine following the transfer.
I have this code working, but during development I noticed that the udma.h provided value for UDMA_INT_SW is 62. The correct value seems to be 60. The relevant parts of my working code are:
tDMAControlTable sUnpackTaskList[kMaxChan];
void UnpackSamples()
{
...
}
void DMAManager::SetupSampleTransfer()
{
...
// Note UDMA_INT_SW in udma.h seems to be incorrect (62)
uDMAIntRegister(60, UnpackSamples);
uDMAChannelAttributeEnable(UDMA_CHANNEL_SW, 0);
}
void DMAManager::TransferSamples(...)
{
...
uDMAChannelScatterGatherSet(UDMA_CHANNEL_SW, 8, sUnpackTaskList, 0);
uDMAChannelEnable(UDMA_CHANNEL_SW);
uDMAChannelRequest(UDMA_CHANNEL_SW);
}
The TM4C1294kcpdt Microcontroller datasheet lists "uDMA Software Channel Transfer" interrupt as 44 which is consistent with 60 as the exception number per the vector table shown in Figure 2-6 (60 = 44 + 16).
It seems unlikely that such an error in the udma.h header has gone unnoticed. Is there something silly I've missed here?