This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have a custom board with Tiva TM4C1294NCPDT. This board will be connected to a iC-MU position encoder which is provided by the client. This encoder supports SSI interface.
I have only clock (PA2) and tx(PA4) of Tiva connected with the encoder. I read from the Tiva 129 data sheet that PA4 can be configured bi-directional mode. Does it means if PA can be used for TX or RX?
My requirement is that I need to read a register called Status0 register of the encoder using SSI.
Can it be achieved ? I have only one pin for data PA4.?
Regards,
Pradeep