Part Number: LAUNCHXL2-RM46
Other Parts Discussed in Thread: HALCOGEN
Hi,
I am working with LaunchPad XL2-RM46 and CCS 8.2.0 (compiler for ARM, TI v18.1.5.LTS). I wrote a RTOS based on a simplification of the freeRTOS. This RTOS use only static allocation of the memory and the assembly code for handling the context switching from a task to another one is the same generate by HALCoGen (04.07.00) for a RM46 processor with freeRTOS. I also use the same interrupts (RTI COMP0, SSI and SVC) for handling the RTOS work.
If I use only the RTOS scheduler with its 3 interrupts, everything works fine. I tryed to create 3 tasks, 2 for blinking the two user's LEDs on the board and 1 for suspending a task or trying other task controllers. Everything is OK. When I try to use other interrupts, for example, for handling PWM signals output with the eTPWM module, the code works fine for some cycles and then I have an abort condition. I am having big trouble to find the source of this problem.
The situation looks a bit strange, because when I run (in debug) the application the first time, I usually have a prefetch abort condition after about 22k times the eTPWM interrupt is triggered, but not always. All the other times, I have a data abort error, exactly after 8188 eTPWM interrupt triggers (there is a counter inside the ISR). I tryed to change the total stack dimension (in the linker file) and the user, IRQ and SVC stacks dimension (updating the _coreInitStackPointer_ function), but it did not fix the issues (and the counter value is always 8188).
Following the relevant registers values when the data abort interrupt is fired:
PC = 0x00000010 (== position of "B _dabort" in the interrupt vector)
SP = R13_ABT = 0x08001F00 (== top of the stack "abortSp" fixed inside the _coreInitStackPointer_ function)
LR = R14_ABT = 0x000002B0
R0 = 0xE8FD9800
CP15_DATA_FAULT_STATUS = 0x00000808 (Reserved value... I don't know the meaning; I checked the Cortex-R4 TRM r1p3, page 129)
CP15_DATA_FAULT_ADDRESS = 0xE8FD97FC ( == R0 - 4)
The LR register point to an instruction in the "portSAVE_CONTEXT" assembly function, inlined in the ISR of the RTOS Tick (RTI Comp0 interrupt), here the Disassembly output:
229 portSAVE_CONTEXT
$C:/*******/src/portAsm.asm:225:247$(), osPortPreemptiveTick():
00000294: F57FF04F dsb sy
00000298: E92D0001 stmdb sp!, {r0}
0000029c: E24DD004 sub sp, sp, #4
000002a0: E84D2000 stmda sp, {sp} ^
000002a4: E8BD0001 ldm sp!, {r0}
000002a8: E9204000 stmdb r0!, {lr}
000002ac: E1A0E000 mov lr, r0
000002b0: E8BD0001 ldm sp!, {r0}
000002b4: E94E7FFF stmdb lr, {r0, r1, r2, r3, r4, r5, r6, r7, r8, r9, r10, r11, r12, sp, lr} ^
000002b8: E24EE03C sub lr, lr, #0x3c
It is clear that the problem is the access to a prohibited address of the memory (0xE8FD97FC), probably because of a corruption of the stack, but I cannot find when and where the stack is corrupted.
The eTPWM ISR change only the value of some eTPWM registers and of a static global variable, not related with the RTOS.
Any suggestions about how to better investigate this problem? Any idea about what could be the error?
Thanks in advance for any help.
PS. I wrote also the code for a MODBUS RTU communication with the SCI interface, using the support of the DMA and N2HET modules. The application use the same RTOS plus DMA and HET interrupts. The MODBUS communication works fine for some messages, than I have the same issues described before (but with different registers values).