This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1:RM46L850PGET, the second pin (GIOA [0]/USB2.0VP/USB-FUNC.RXDPI) can not be controlled by software programming when using the open-leak output mode, that is, the indicator lights are often on; other output modes, such as push-pull output, are OK, please analyze the reasons.
2: At first, 40 boards use the output mode of opening and leaking. The indicator lights are programmable control. After aging for a period of time, two of the 40 boards appear the situation described above at 1 point.
3: The current of the test pin is 6mA.
4: The following is the schematic diagram:
Hi,
If Output Buffer Drive Strength (sink/source) of GIOA pins is 2mA,why GIOA[0]( I_red=6mA) is normal,GIOA[1](I_green=3.73mA) is damaged?
(1),we use GIOA[0](pin 2) ,open drain to control Red LED,test I_red=6mA;
GIOA[1](pin 5) ,open drain to control Green LED,test I_green=3.73mA;
GIOA[2](pin 9) ,open drain to control BlueLED,test I_blue=3mA;
Now GIOA[0]and GIOA[2] are normal,but GIOA[1] is damaged,that is very trange.
(2),Output Buffer Drive Strength (sink/source) of GIOA pins is 2mA,this is too small,normally MCU input current 10mA,why your MCU is only 2mA?
(3),Your datasheet present,Input clamp current max is 10mA,and I_CCIO max is 10mA,why GIOA[1](I_green=3.73mA) is damaged?
Thanks!
Hello,
You should test whether pins are damaged. If you are measuring 6, 3mA and 3.73 mA then LEDs should lit!
(1),we use GIOA[0](pin 2) ,open drain to control Red LED,test I_red=6mA;
GIOA[1](pin 5) ,open drain to control Green LED,test I_green=3.73mA;
GIOA[2](pin 9) ,open drain to control BlueLED,test I_blue=3mA;
Now GIOA[0]and GIOA[2] are normal,but GIOA[1] is damaged,that is very trange.
--> TI recommended conditions are stated in Datasheet. It is not recommended to use the device in where conditions exceeds recommended.
(2),Output Buffer Drive Strength (sink/source) of GIOA pins is 2mA,this is too small,normally MCU input current 10mA,why your MCU is only 2mA?
--> According to Datasheet Output Buffer Drive Strength for GIOA is 2mA. You should use buffer to drive load more than this.
(3),Your datasheet present,Input clamp current max is 10mA,and I_CCIO max is 10mA,why GIOA[1](I_green=3.73mA) is damaged?
--> Input clamp current is the current that flows through ESD protection diodes.
--> Iccio max is maximum supply current that the device will consume from Vccio when there is no DC load.
Best regards,
Miro