Part Number: TM4C1294NCPDT
I am planning to use the QSSI on the TivaC to connect a multi-channel ADC.
I need some help understanding Relationship between the frame sync and the data in receive mode.
What happens if the frame is longer than the data size? I checked here but wasn't clear to me.
Ideally I would have 4 bit wide data that is 64 bits long (256 bits per frame),
That would produce 32 bytes DMA’d direct to pin-pong ram.
Any app notes?
I have two Tiva dev boards so are going to try some things so any examples that would help me get started with evaluating this would be much appreciated :)