Other Parts Discussed in Thread: TM4C123GH6PM
Hello ,
Im trying to send some data via UART1 serial from tiva-c launchpad and it seems like the data is send but the interrupt is not called.
Here is my code
#include <stdbool.h>
#include <stdint.h>
#include <inc/hw_memmap.h>
#include <driverlib/sysctl.h>
#include <driverlib/gpio.h>
#include <inc/hw_ints.h>
#include <driverlib/interrupt.h>
#include <driverlib/uart.h>
#include "driverlib/pin_map.h"
void UARTIntHandler(void);
int main()
{
int data=1;
SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);
//enable peripheral clock for UART0
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART1);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
GPIOPinConfigure( GPIO_PB0_U1RX );
GPIOPinConfigure( GPIO_PB1_U1TX );
GPIOPinTypeUART( GPIO_PORTB_BASE , GPIO_PIN_0 | GPIO_PIN_1 );
//disable UART0
UARTDisable(UART1_BASE);
//configure divisor and format
UARTConfigSetExpClk(UART1_BASE, SysCtlClockGet(), 2400, (UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE));
//enable FIFO
UARTFIFOEnable(UART1_BASE); //is enabled automatically when UARTEnable() is called
//enable individual UART interrupt source
UARTIntEnable(UART1_BASE, UART_INT_RX | UART_INT_RT);
//enable UART0 interrupt
UARTIntRegister(UART1_BASE, UARTIntHandler);
//IntEnable(INT_UART0);
//enable processor interrupt
IntMasterEnable();
//enable UART0
UARTEnable(UART1_BASE);
UARTCharPut(UART1_BASE,data) ;
while(1);
}
void UARTIntHandler(void)
{
uint32_t UIstatus = UARTIntStatus(UART0_BASE, true);
UARTIntClear(UART0_BASE, UIstatus);
}