This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello ,
Im trying to send some data via UART1 serial from tiva-c launchpad and it seems like the data is send but the interrupt is not called.
Here is my code
#include <stdbool.h> #include <stdint.h> #include <inc/hw_memmap.h> #include <driverlib/sysctl.h> #include <driverlib/gpio.h> #include <inc/hw_ints.h> #include <driverlib/interrupt.h> #include <driverlib/uart.h> #include "driverlib/pin_map.h" void UARTIntHandler(void); int main() { int data=1; SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ); //enable peripheral clock for UART0 SysCtlPeripheralEnable(SYSCTL_PERIPH_UART1); SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB); GPIOPinConfigure( GPIO_PB0_U1RX ); GPIOPinConfigure( GPIO_PB1_U1TX ); GPIOPinTypeUART( GPIO_PORTB_BASE , GPIO_PIN_0 | GPIO_PIN_1 ); //disable UART0 UARTDisable(UART1_BASE); //configure divisor and format UARTConfigSetExpClk(UART1_BASE, SysCtlClockGet(), 2400, (UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE)); //enable FIFO UARTFIFOEnable(UART1_BASE); //is enabled automatically when UARTEnable() is called //enable individual UART interrupt source UARTIntEnable(UART1_BASE, UART_INT_RX | UART_INT_RT); //enable UART0 interrupt UARTIntRegister(UART1_BASE, UARTIntHandler); //IntEnable(INT_UART0); //enable processor interrupt IntMasterEnable(); //enable UART0 UARTEnable(UART1_BASE); UARTCharPut(UART1_BASE,data) ; while(1); } void UARTIntHandler(void) { uint32_t UIstatus = UARTIntStatus(UART0_BASE, true); UARTIntClear(UART0_BASE, UIstatus); }
Hello Bob ,
I have modified my code but the IntEnable do not solved this. The thing was that i had connected to PB1( Tx ) and PB0( Rx ) pins two wires from a Logic analyzer and it seems like the interrupt is not called if the pins are connected to the wires. Nevertheless i also activated all kinds of uart interrupts, i will let here my new code. The question is why the interrupt is now called but not with Tx reason and why if i connected the wires to PB1 and PB0 pins the interrupt is not called anymore. Also a thing to know is that im using an tiva-c with an tm4c123gh6pm microcontroller.
#include <stdbool.h> #include <stdint.h> #include <inc/hw_memmap.h> #include <driverlib/sysctl.h> #include <driverlib/gpio.h> #include <inc/hw_ints.h> #include <driverlib/interrupt.h> #include <driverlib/uart.h> #include "driverlib/pin_map.h" void UARTIntHandler(void); volatile int flag = 1 ; int main() { int data=1; SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ); //enable peripheral clock for UART0 SysCtlPeripheralEnable(SYSCTL_PERIPH_UART1); SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB); GPIOPinConfigure( GPIO_PB0_U1RX ); GPIOPinConfigure( GPIO_PB1_U1TX ); GPIOPinTypeUART( GPIO_PORTB_BASE , GPIO_PIN_0 | GPIO_PIN_1 ); //disable UART0 UARTDisable(UART1_BASE); //configure divisor and format UARTConfigSetExpClk(UART1_BASE, SysCtlClockGet(), 2400, (UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE)); //enable FIFO UARTFIFOEnable(UART1_BASE); //is enabled automatically when UARTEnable() is called //enable individual UART interrupt source UARTIntEnable( UART1_BASE, UART_INT_DMATX | UART_INT_DMARX | UART_INT_9BIT | UART_INT_OE | UART_INT_BE | UART_INT_PE | UART_INT_FE | UART_INT_RT | UART_INT_TX | UART_INT_RX | UART_INT_DSR | UART_INT_DCD | UART_INT_CTS | UART_INT_RI ); UARTIntRegister(UART1_BASE, UARTIntHandler); //enable processor interrupt IntMasterEnable(); IntEnable(INT_UART1); UARTEnable(UART1_BASE); UARTCharPut(UART1_BASE,data) ; while(1); } void UARTIntHandler(void) { uint32_t UIstatus = UARTIntStatus(UART1_BASE, true); UARTIntClear(UART1_BASE, UIstatus); flag = 0 ; }
Here you can see why the interrupt is called
The interrupt status flags you are receiving are Break error, Framing error and Receive time out. That makes me suspect that you do not have a valid signal attached to PB0. Is it left floating? When you have a logic analyzer attached to that pin, the leakage current from the logic analyzer input probably keeps the level high enough that it does not trigger the UART RX.
You are not getting a TX interrupt because you are using the FIFO mode with the FIFO level set to 1/2. That means you will get a TX interrupt when the level of the TX FIFO goes from 9 characters left to transmit to 8 characters left to transmit (8 empty spots in the TX FIFO). In your example, you never attempt to transmit more than one character. Therefore the FIFO never goes above half full, so it never generates an interrupt for transitioning from above half full to half full. If you want to generate a TX interrupt when the last character has completed transmission, then call:
UARTTxIntModeSet(UART1_BASE, UART_TXINT_MODE_EOT);