Part Number: EK-TM4C1294XL
Other Parts Discussed in Thread: TM4C1294NCPDT
Dear Sir,
With the help of enet_s2e example code, I was able to pass my data through the ethernet to the UART specified. But as the micro-controller TM4C1294NCPDT supports 8 UARTs , so can I use more than the two ports connected with other UARTs (exclusive of the specified ports at port numbers 23 and 26 respectively) which would really be helpful for my application.
Thanks in Advance,