Part Number: TM4C1290NCPDT
Tool/software: Code Composer Studio
Hello,
I've been trying to get the EPI on the TM4C129 working in muxed 8bit host bus mode but having zero luck. Snippets of the code are below, please let me know what I'm doing wrong. On the scope I monitor the AD0, ALE, WRn, RDn and nothing is toggling.
///////////////////////////////////////////////
//from the linker file
//////////////////////////////////////////////
--retain=g_pfnVectors
#define NOINIT_RAM_SIZE 0x10
#define FPGA_BASE 0xA0000000
MEMORY
{
FLASH (RX) : origin = 0x00004400, length = 0x00100000 - 0x4400
SRAM (RWX) : origin = 0x20000000, length = 0x00040000 - NOINIT_RAM_SIZE
NOINIT_RAM (RWX) : origin = end(SRAM), length = NOINIT_RAM_SIZE
/* Application uses external FPGA memory mapped resigters */
FPGA (RWX) : origin = FPGA_BASE, length = 0x00010000
}
SECTIONS
{
.intvecs: > 0x00004400
.text : > FLASH
.const : > FLASH
.cinit : > FLASH
.pinit : > FLASH
.init_array : > FLASH
.vtable : > 0x20000000
.data : > SRAM
.bss : > SRAM
.sysmem : > SRAM
.stack : > SRAM
.external : > FPGA
.noinit : > NOINIT_RAM, type = NOINIT
}
__STACK_TOP = __stack + 512;
///////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
//EPI initilization
///////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
///////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
// The following specifies the GPIO pins used by the EPI bus when
// configured in HostBus8 mode. using AD[0..7] & A[8..15], WRn, RDn & ALE
///////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
#define EPI_PORTA_PINS 0xC0 //pins[7:6] used for Addr A[9:8]
#define EPI_PORTB_PINS 0x04 //pin[2] used for RD_strobe
#define EPI_PORTC_PINS 0xF0 //pins[4:7] used for AddrData AD[7:4]
#define EPI_PORTD_PINS 0x00 //not used by EPI
#define EPI_PORTE_PINS 0x00 //not used by EPI
#define EPI_PORTF_PINS 0x00 //not used by EPI
#define EPI_PORTG_PINS 0x03 //pins[0:1] used for Addr A[11:10]
#define EPI_PORTH_PINS 0x0F //pins[3:0] used for AddrData AD[3:0]
#define EPI_PORTJ_PINS 0x00 //not used by EPI
#define EPI_PORTK_PINS 0x00 //not used by EPI
#define EPI_PORTL_PINS 0x07 //pins[2:0] used for Addr[18:16]
#define EPI_PORTM_PINS 0x0F //pins[0:3] used for Addr[15:12]
#define EPI_PORTN_PINS 0x00 //not used by EP
#define EPI_PORTP_PINS 0x0C //pin[2] used for WR_strobe & pin[3] used for ALE
#define EPI_PORTQ_PINS 0x00 //not used by EPI
// Enable all GPIO banks.
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOG);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOH);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOJ);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOK);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOL);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOM);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOP);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOQ);
/*
GPIOPadConfigSet(GPIO_PORTA_BASE, EPI_PORTA_PINS, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
GPIODirModeSet(GPIO_PORTA_BASE, EPI_PORTA_PINS, GPIO_DIR_MODE_HW);
GPIOPadConfigSet(GPIO_PORTB_BASE, EPI_PORTB_PINS, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
GPIODirModeSet(GPIO_PORTB_BASE, EPI_PORTB_PINS, GPIO_DIR_MODE_HW);
GPIOPadConfigSet(GPIO_PORTC_BASE, EPI_PORTC_PINS, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
GPIODirModeSet(GPIO_PORTC_BASE, EPI_PORTC_PINS, GPIO_DIR_MODE_HW);
GPIOPadConfigSet(GPIO_PORTD_BASE, EPI_PORTD_PINS, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
GPIODirModeSet(GPIO_PORTD_BASE, EPI_PORTD_PINS, GPIO_DIR_MODE_HW);
GPIOPadConfigSet(GPIO_PORTE_BASE, EPI_PORTE_PINS, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
GPIODirModeSet(GPIO_PORTE_BASE, EPI_PORTE_PINS, GPIO_DIR_MODE_HW);
GPIOPadConfigSet(GPIO_PORTF_BASE, EPI_PORTF_PINS, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
GPIODirModeSet(GPIO_PORTF_BASE, EPI_PORTF_PINS, GPIO_DIR_MODE_HW);
GPIOPadConfigSet(GPIO_PORTG_BASE, EPI_PORTG_PINS, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
GPIODirModeSet(GPIO_PORTG_BASE, EPI_PORTG_PINS, GPIO_DIR_MODE_HW);
GPIOPadConfigSet(GPIO_PORTH_BASE, EPI_PORTH_PINS, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
GPIODirModeSet(GPIO_PORTH_BASE, EPI_PORTH_PINS, GPIO_DIR_MODE_HW);
GPIOPadConfigSet(GPIO_PORTJ_BASE, EPI_PORTJ_PINS, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
GPIODirModeSet(GPIO_PORTJ_BASE, EPI_PORTJ_PINS, GPIO_DIR_MODE_HW);
GPIOPadConfigSet(GPIO_PORTK_BASE, EPI_PORTK_PINS, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
GPIODirModeSet(GPIO_PORTK_BASE, EPI_PORTK_PINS, GPIO_DIR_MODE_HW);
GPIOPadConfigSet(GPIO_PORTL_BASE, EPI_PORTL_PINS, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
GPIODirModeSet(GPIO_PORTL_BASE, EPI_PORTL_PINS, GPIO_DIR_MODE_HW);
GPIOPadConfigSet(GPIO_PORTM_BASE, EPI_PORTM_PINS, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
GPIODirModeSet(GPIO_PORTM_BASE, EPI_PORTM_PINS, GPIO_DIR_MODE_HW);
GPIOPadConfigSet(GPIO_PORTN_BASE, EPI_PORTN_PINS, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
GPIODirModeSet(GPIO_PORTN_BASE, EPI_PORTN_PINS, GPIO_DIR_MODE_HW);
GPIOPadConfigSet(GPIO_PORTP_BASE, EPI_PORTP_PINS, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
GPIODirModeSet(GPIO_PORTP_BASE, EPI_PORTP_PINS, GPIO_DIR_MODE_HW);
GPIOPadConfigSet(GPIO_PORTQ_BASE, EPI_PORTQ_PINS, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
GPIODirModeSet(GPIO_PORTQ_BASE, EPI_PORTQ_PINS, GPIO_DIR_MODE_HW);
*/
//
// Enable pin PH0 for EPI0 EPI0S0
//
MAP_GPIOPinConfigure(GPIO_PH0_EPI0S0);
GPIOPinTypeEPI(GPIO_PORTH_BASE, GPIO_PIN_0);
//
// Enable pin PH1 for EPI0 EPI0S1
//
MAP_GPIOPinConfigure(GPIO_PH1_EPI0S1);
GPIOPinTypeEPI(GPIO_PORTH_BASE, GPIO_PIN_1);
//
// Enable pin PH2 for EPI0 EPI0S2
//
MAP_GPIOPinConfigure(GPIO_PH2_EPI0S2);
GPIOPinTypeEPI(GPIO_PORTH_BASE, GPIO_PIN_2);
//
// Enable pin PH3 for EPI0 EPI0S3
//
MAP_GPIOPinConfigure(GPIO_PH3_EPI0S3);
GPIOPinTypeEPI(GPIO_PORTH_BASE, GPIO_PIN_3);
//
// Enable pin PC7 for EPI0 EPI0S4
//
MAP_GPIOPinConfigure(GPIO_PC7_EPI0S4);
GPIOPinTypeEPI(GPIO_PORTC_BASE, GPIO_PIN_7);
//
// Enable pin PC6 for EPI0 EPI0S5
//
MAP_GPIOPinConfigure(GPIO_PC6_EPI0S5);
GPIOPinTypeEPI(GPIO_PORTC_BASE, GPIO_PIN_6);
//
// Enable pin PC5 for EPI0 EPI0S6
//
MAP_GPIOPinConfigure(GPIO_PC5_EPI0S6);
//GPIOPinTypeEPI(GPIO_PORTC_BASE, GPIO_PIN_5);
//
// Enable pin PC4 for EPI0 EPI0S7
//
MAP_GPIOPinConfigure(GPIO_PC4_EPI0S7);
GPIOPinTypeEPI(GPIO_PORTC_BASE, GPIO_PIN_4);
//
// Enable pin PA6 for EPI0 EPI0S8
//
MAP_GPIOPinConfigure(GPIO_PA6_EPI0S8);
GPIOPinTypeEPI(GPIO_PORTA_BASE, GPIO_PIN_6);
//
// Enable pin PA7 for EPI0 EPI0S9
//
MAP_GPIOPinConfigure(GPIO_PA7_EPI0S9);
GPIOPinTypeEPI(GPIO_PORTA_BASE, GPIO_PIN_7);
//
// Enable pin PG1 for EPI0 EPI0S10
//
MAP_GPIOPinConfigure(GPIO_PG1_EPI0S10);
GPIOPinTypeEPI(GPIO_PORTG_BASE, GPIO_PIN_1);
//
// Enable pin PG0 for EPI0 EPI0S11
//
MAP_GPIOPinConfigure(GPIO_PG0_EPI0S11);
GPIOPinTypeEPI(GPIO_PORTG_BASE, GPIO_PIN_0);
//
// Enable pin PM3 for EPI0 EPI0S12
//
MAP_GPIOPinConfigure(GPIO_PM3_EPI0S12);
GPIOPinTypeEPI(GPIO_PORTM_BASE, GPIO_PIN_3);
//
// Enable pin PM2 for EPI0 EPI0S13
//
MAP_GPIOPinConfigure(GPIO_PM2_EPI0S13);
GPIOPinTypeEPI(GPIO_PORTM_BASE, GPIO_PIN_2);
//
// Enable pin PM1 for EPI0 EPI0S14
//
MAP_GPIOPinConfigure(GPIO_PM1_EPI0S14);
GPIOPinTypeEPI(GPIO_PORTM_BASE, GPIO_PIN_1);
//
// Enable pin PM0 for EPI0 EPI0S15
//
MAP_GPIOPinConfigure(GPIO_PM0_EPI0S15);
GPIOPinTypeEPI(GPIO_PORTM_BASE, GPIO_PIN_0);
//
// Enable pin PL0 for EPI0 EPI0S16
//
MAP_GPIOPinConfigure(GPIO_PL0_EPI0S16);
GPIOPinTypeEPI(GPIO_PORTL_BASE, GPIO_PIN_0);
//
// Enable pin PL1 for EPI0 EPI0S17
//
MAP_GPIOPinConfigure(GPIO_PL1_EPI0S17);
GPIOPinTypeEPI(GPIO_PORTL_BASE, GPIO_PIN_1);
//
// Enable pin PL2 for EPI0 EPI0S18
//
MAP_GPIOPinConfigure(GPIO_PL2_EPI0S18);
GPIOPinTypeEPI(GPIO_PORTL_BASE, GPIO_PIN_2);
//
// Enable pin PB3 for EPI0 EPI0S28
//
MAP_GPIOPinConfigure(GPIO_PB3_EPI0S28);
GPIOPinTypeEPI(GPIO_PORTB_BASE, GPIO_PIN_3);
//
// Enable pin PN2 for EPI0 EPI0S29
//
MAP_GPIOPinConfigure(GPIO_PP2_EPI0S29);
GPIOPinTypeEPI(GPIO_PORTP_BASE, GPIO_PIN_2);
//
// Enable pin PN3 for EPI0 EPI0S30
//
MAP_GPIOPinConfigure(GPIO_PP3_EPI0S30);
GPIOPinTypeEPI(GPIO_PORTP_BASE, GPIO_PIN_3);
// Enable the EPI peripheral
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_EPI0);
// Set the EPI operating mode for FPGA iFace
// The values used here set the EPI to run at the system_clock/16 = 7.5MHz
// with first 8 bits of AddrData muxed
// two wait states for rd/wr, this is wait 0 which is two EPI clocks
EPIModeSet(EPI0_BASE, EPI_MODE_HB8);
EPIDividerSet(EPI0_BASE, 16);
//EPIConfigHB8Set(EPI0_BASE, (EPI_HB8_MODE_ADMUX | EPI_HB8_WRWAIT_0 |
//EPI_HB8_RDWAIT_0 | EPI_HB8_WORD_ACCESS), 0);
EPIConfigHB8Set(EPI0_BASE, (EPI_HB8_MODE_ADMUX | EPI_HB8_WRWAIT_0 |
EPI_HB8_RDWAIT_0), 0);
EPIAddressMapSet(EPI0_BASE, EPI_ADDR_RAM_SIZE_64KB | EPI_ADDR_PER_BASE_A);
///////////////////////////////////////////////////////////////////////////////
// simple test usage
///////////////////////////////////////////////////////////////////////////////
#define FPGA_BASE 0xA0000000
volatile uint16_t *FPGAptr = ((uint16_t *)FPGA_BASE);
int main(void)
{
uint32_t i;
for (i = 0; i < 32768; i++)
{
FPGAptr[i] = i;
}
for (i = 0; i < 32768; i++)
{
ptr[i] = FPGAptr[i];
}
}