This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
in my software a division by zero doesn't generate an undefined instruction exception.
In the cortex R4 Reference Manual there is a DZ (divide by zero) bit to generate an undefined instruction exception, in the System Control Register. By default this bit is zero (do not generate an Undefined instruction exception).
In the RM48 Reference Manual I don't find the DZ bit.
How to generate an exception when I divide a value by zero ?
Thanks
Eric
Hello,
I found a thread similar to yours. Please check whether it helps.
Help:TMS570LS3137 No Divide zero abort - Arm-based microcontrollers forum - Arm-based microcontrollers...
Hello
DZ bit is enable by these lines (from udiv.asm)
MRC p15, #0,r3,c1,c0,#0
orr r3,r3,#0x80000
MCR p15, #0,r3,c1,c0,#0
I have included these lines in my software and it works fine for integer values. I have an exception if I divide by zero an integer.
However it doesn't work for float values, I don't have an exception.
How to have an exception by dividing a float value by zero ?
Thanks
Eric
Eric,
There is a secondary auxiliary control register which has a bit called DZC. This bit is 0 by default, which masks the output of a floating-point divide-by-zero exception. This bit must be set to '1' to enable the output of this exception. See the Cortex-R4F TRM for more details.
Regards, Sunil